RealSense Support

D415 RGB Resolution

Comments

2 comments

  • MartyG

    Hi Eskimos Nl+realsense  The D415's default RGB resolution is 1280x720.  If you are using the RealSense Viewer tool then you can choose 1920x1080 from the resolution selection drop-down in the RGB section of the Viewer's options side-panel.

     

     

    If you are writing your own program then you can override the default and set your chosen resolution using a cfg stream configuration line.  For example:

     

    cfg.enable_stream(rs.stream.color, 1920, 1080, rs.format.rgb8, 30)
    0
    Comment actions Permalink
  • Eskimos Nl+realsense

    Thank you.

    0
    Comment actions Permalink

Please sign in to leave a comment.