RealSense Support

We would like to request image height test data per FOV.

Comments

2 comments

  • MartyG

    Hi Comme002  You can retrieve image information for a particular sensor type at a particular resolution using the RealSense SDK's rs-enumerate-devices tool and launching the tool in calibration information mode with the command rs-enumerate-devices -c

     

    The tool generates a long list of the camera's extrinsic and intrinsic information in a terminal window so that you can scroll through it to find the information that you want.

     

     

    In regards to sensor angle, all of the sensors point forwards from the front of the camera.  The field of view (FOV) of each sensor is slightly offset horizontally from each other due to their different physical location on the camera front.

    0
    Comment actions Permalink
  • MartyG

    On the D455 camera model the IR and RGB sensors have a similar field of view size, whilst on the D435i model the RGB sensor has a smaller field of view.

    0
    Comment actions Permalink

Please sign in to leave a comment.