Long Distance Vision Application.
Hi,
I am looking into an application to detect changes in infrared signals day and night. Can someone tell me what is the typical distance one could cover with this technology?
What will be the field of vision at this distance?
Thanks
Bharat
-
Hi Bharat Gupta If long range depth sensing is required then the RealSense D455 will be the best choice of camera model, as it can depth-sense up to 20 meters. The link below has a demonstration of this.
In regard to infrared sensing, RealSense cameras can see much further as the depth distance limitation does not apply to infrared and RGB. If you only need infrared and will not be using depth sensing then any RealSense camera model except D405 (the short-range model with high-quality images) should meet your long-distance requirements.
If you require a wide field of view then the D415 model will not be suitable for your needs.
If you choose D435 / D435i / D435f / D435if or the D455 / D455f then the field of view values for the infrared sensor in these models are:
Horizontal Field of View 90
Vertical Field of View 64
Diagonal Field of View 98 -
Hi MartyG,
Thanks for getting back. Your answer is helpful, but I was kind of looking at distances of tens of KM,. I can do 360 degrees by installing 4 cameras based on the information provided. I really need a longer range and the application is outdoor-so it has to work in -40 degree centigrade to +55 degree ambient temperatures.
I am not sure, from what little I have read about the system, it will be suitable. What do you think?
-
Apologies for posting one paragraph at a time. The site will not list the comment otherwise right now.
The temperature that the outer casing of the camera is exposed to will have an effect on its internal operating temperature. For example, an Intel lab test found that if the outer casing temperature does not exceed 44 degrees C then the internal operating temperature should not exceed 60 degrees C.
-
Laser shut-off does not prevent the camera from operating, though the infrared image will likely be darker and the camera would not be able to provide an infrared image at night unless an external infrared light source such as an IR illuminator lamp was installed nearby so that the camera could use that light source instead of the laser light.
-
If the ambient temperature was sub-zero then the internal operating temperature would likely not be as low as the outer environment because of the heat generated from the electronics. Maximizing the Laser Power setting of the camera could also help to raise its internal temperature.
Please sign in to leave a comment.

Comments
11 comments