RealSense Support

A-factor left as 0.0 in preset files?

Comments

1 comment

  • MartyG

    Hi Toni Divic  The json parameter for A-Factor is param-amplitude-factor, which can be defined in a json camera configuration file like this:

    "param-amplitude-factor": "0"

     

    The default value is '0'.  If a custom json preset is exported from the RealSense Viewer tool then the default that is saved into the json for the param-amplitude-factor setting is also '0' unless the value is manually changed in the Viewer's options side-panel before exporting the json.  This setting can be found under Stereo Module > Advanced Controls > Disparity Modulation

     

    My interpretation of the advice in the subpixel linearity guide is that the 0.08 value is a recommendation by the authors of the paper based on their test results, and that '0' officially remains the default value for the A-Factor but RealSense users are free to experiment with the setting to see if it improves their results.

    0
    Comment actions Permalink

Please sign in to leave a comment.