RealSense Support

Cannot access the L515 camera using the python pyrealsense2 library on a Rasberry Pi4

Comments

10 comments

  • Wai Fook Wan

    Hello Customer,

    Thanks for reaching out to us.

     

    Did you install the package from https://pypi.org/project/pyrealsense2/ or build the package from source?

     

    To use the Python wrapper for Intel® RealSense™ SDK, please follow the steps in the following link:

    https://github.com/IntelRealSense/librealsense/blob/development/doc/installation_raspbian.md#raspbianraspberrypi3-installation

     

     

    Regards,

    Wan

    Intel Customer Support

     

     

    0
    Comment actions Permalink
  • 7159486

    Yes, we installed the package from there, using the pip install pyrealsense2 command. Regarding the second point, we installed it according to this tutorial .

    Could you please tell me

    1. How to install pyrealsense2 from sourse?
    2. Do you have a tutorial on installing programs for Pi4 8gb and RealSense L515 combination?

    0
    Comment actions Permalink
  • Wai Fook Wan

    Thanks for your information.

    To install pyrealsense2 from the source, please follow the steps in Raspbian Installation with some minor changes:

     

    When installing protobuf, please git clone the following branch:

    git clone --depth 1 -b v3.10.0 https://github.com/protocolbuffers/protobuf.git

    0
    Comment actions Permalink
  • 7159486

    Thank you very much for the answer! Can you tell me what version of python should be installed?

    0
    Comment actions Permalink
  • Wai Fook Wan

    Hello,

    You may use the default Python version that has been installed in your Raspberry Pi.

    0
    Comment actions Permalink
  • 7159486

    I need a proven working link to work with D435 or L515 Intel Real Sense cameras on Rasbery Pi4 (arm64).
    That is, you need a working sequence of commands for a specific OS (please specify the version).
    Minimum questions:
    1. What version of python do you need?
    2. What version of Cmake do you need?
    3. What version of gcc is needed?
    4. What packages are initially needed for bare linux (apt-get install ...)?
    5. What version of protobuf and how to build it from source?
    6. Do I need TBB, which version and how to assemble?
    7. What version of OpenCV should be installed and how to build from source?
    8. What version of SDK\librealsense should be installed and how?
    9. How to build and which version of pyrrealsense
    10. What additional dependencies need to be installed between all these programs?

    I have already tried 3-4 instructions and everywhere there is a Segmentation foul, which occurs in the depths of the SDK.

    0
    Comment actions Permalink
  • Wai Fook Wan

    Hello Customer,

    Let me check with relevant team and I'll update you at the earliest.

     

     

    Regards,

    Wan

    0
    Comment actions Permalink
  • Wai Fook Wan

    Hello Customer, 

    Did you encounter Segmentation Fault when using your custom Python code?

    I've validated the steps in Raspbian Installation and I'm able to run Tutorial 1 from Sample Code for Intel® RealSense™ Python Wrapper.

    Could you please run Tutorial 1 from Sample Code for Intel® RealSense™ Python Wrapper and see if you encounter Segmentation Fault?

     

     

    Regards,

    Wan

    0
    Comment actions Permalink
  • 7159486

    It worked, thank you!

    0
    Comment actions Permalink
  • Wai Fook Wan

    Hello customer,

    Thanks for your question.

     

    If you need any additional information from Intel, please submit a new question as this thread will no longer be monitored.

     

     

    Regards,

    Wan

    0
    Comment actions Permalink

Please sign in to leave a comment.