RealSense Support

Basic Install - I installed the USB driver, but the software still can't see the camera

Comments

1 comment

  • MartyG

    Hi Steven Klems  I am not aware of a requirement for a special driver for the Newnex fiber optic cable.  In the YouTube video demonstration at the link below, Newnex change seamlessly from a 20 m USB connection to a 100 m fiber one.

    https://www.youtube.com/watch?v=GLQgR1jT04M

     

    Have you installed the full RealSense SDK for Windows by downloading and running the Intel.RealSense.SDK-WIN10 installer file from the 'Assets' file list at the bottom of the page at the link below, please?

    https://github.com/IntelRealSense/librealsense/releases/tag/v2.54.1

     

     

    The SDK and the RealSense Viewer tool that the installer laces a launch shortcut icon for on the Windows desktop will enable you to test the camera. The drivers for the camera are already automatically installed into the Windows Device Manager when the camera is inserted into the USB port though.

     

    Also, which RealSense camera model are you using please?  If it is a D457 then you need to move the position of a mode switch in the camera casing in order for it to be detected on a USB connection, as described at the link below.

    https://support.intelrealsense.com/hc/en-us/community/posts/14840675121043/comments/14843232242835

    0
    Comment actions Permalink

Please sign in to leave a comment.