RealSense Support

D455 'Device Enumeration Failed' after rolling back firmware

Comments

2 comments

  • Pcray

    Is there any new information on this issue or how to resolve?

    I am having the same problem. I need to install 5_12_7_100 but am having the issue described here every time I do.

    I was able to restore the camera to working order, but that leaves me running the newer firmware version 5_15_0_2. Downgrading from there takes me back to the same problem described in this post.

    0
    Comment actions Permalink
  • MartyG

    Hi Pcray  If you are using a D455 like Jason Delevan then the firmware release notes for the 'Production' firmware state that 5.12.7.100 no longer supports D455.

    https://dev.intelrealsense.com/docs/recommended-production-camera-configurations

     

    'Production' firmwares are ones that Intl has validated as being stable and reliable enough to use in commercial products and critical applications.

     

     

    The first firmware which supports D455 is 5.13.0.50, which is also a Production class firmware.  So if you have a D455 then 5.13.0.50 is the absolute oldest firmware that can be used.

     

    5.13.0.50 was designed for use with SDK versions 2.50.0 and 2.51.1, whilst 5.15.0.2 is designed for use with SDK 2.54.1. 

    0
    Comment actions Permalink

Please sign in to leave a comment.