RealSense Support

Comments

1 comment

  • MartyG

    Yes, RealSense can use multiple camera (two or more).  An easy way to test this is to use the free RealSense Viewer tool and add additional cameras using the Add Source button at the top of the Viewer's options side-panel.

    0
    Comment actions Permalink

Please sign in to leave a comment.