RealSense Support

Loading of 16 Intel real sense D455 cameras

Comments

3 comments

  • MartyX Grover

    Hi P Landerouin  Could you provide information about the questions below, please?

     

    -  Which computer / computing device are you using?  (PC, Raspberry Pi, Nvidia Jetson, etc)

    -  Are you using the D455 cameras in the RealSense Viewer tool or in an application that you have created yourself?

    -  If it is an application that you have created yourself, are you using poll_for_frames() to retrieve the camera frames instead of wait_for_frames() ?  For control of multiple cameras by a single application, use of poll_for_frames() is recommended in combination with using sleep periods to control when to put the CPU to sleep in order to prevent the CPU usage from maximizing to 100%.  Further information about this can be found in the link below.

    https://github.com/IntelRealSense/librealsense/issues/2422#issuecomment-423254709

    0
    Comment actions Permalink
  • P Landerouin

    Thank you for the answer. It is on a PC, on a application I created in C# (WPF). For my project I used the C# library intel.realSense.dll and realsense2.dll. 

    The trouble happen exactly in the piece of code just under.

    cfg.EnableDevice(sn);
    cfg.EnableStream(Stream.Depth, 848, 480, Format.Z16, depthFrameRate);
    cfg.EnableStream(Stream.Color, 848, 480, Format.Rgb8, colorFrameRate);

    pipeline = new Pipeline();

    pp = pipeline.Start(cfg);  //This line takes very much time

    Ok I will try to use poll_for_frame().

     

    // Start streaming with Json configuration
    pp = pipeline.Start(cfg);

    0
    Comment actions Permalink
  • MartyX Grover

    Could you try using ctx.QueryDevices() in your script like in the C# multicam example in the link below and see whether it improves performance?

    https://github.com/IntelRealSense/librealsense/issues/3432#issuecomment-472570380

    QueryDevices() can be used to automatically generate a list of all attached cameras.

    0
    Comment actions Permalink

Please sign in to leave a comment.