RealSense Support

saving image captured with f455 camera in linux

Comments

6 comments

  • Yu-Chern Peh

    Hello,

    The exact frames used during enrolling and authentication cannot be captured. Only Preview images can be extracted.

    RealSenseID allows Dumping of bitmaps from the Preview in png and RAW format. This functionality is implemented in C# for the RSID Viewer application in the FrameDumper.cs class. The RAW files are not viewable. They are meant to be used for debugging purposes by the RealSense ID engineering team.

    You have access to the Preview image and can save it. Unfortunately, this functionality is currently demonstrated in the C# Preview wrapper but it can be implemented in C/C++  by the developer. Can have a look at this Preview wrapper in C


    Regards,
    Yu-Chern 
    Intel Customer Support

    0
    Comment actions Permalink
  • 191129107

    Hi Yu-Chern Peh

    Thanks for your answer, I can't see the sample images because "rsid-preview" is not active on Linux. When I try to run enroll.cc in the sample codes, I get the error "Undefined reference for RealSenseID::FaceAuthenticator::FaceAuthenticator()". Would you help me with this topic?

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hello,

     

    In order to run samples, you have to build with the command: cmake -DRSID_SAMPLES=1 .. 

    After building, you will find the samples in bin directory.

     

     

    Regards,
    Yu-Chern 
    Intel Customer Support

    0
    Comment actions Permalink
  • 191129107

    Hi Yu-Chern Peh

    I recompiled as you said. Then I ran the "./faces-cpp-sample" example that was created in the "bin" folder and saw the bound box values of the face in the output. However, I want to see the original image taken from the camera and draw the found bound box value on it.
    Here is the output of the example I mentioned:

    Can you help with this.

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hello,

    Try to recompile with preview enabled: cmake -DRSID_PREVIEW=1 -DRSID_SAMPLES=1 .. 


    Regards,
    Yu-Chern 
    Intel Customer Support

    0
    Comment actions Permalink
  • 191129107

    Hi Yu-Chern Peh

    Thank you for your answer, I was able to see the frames after compiling as you said. But can we have a chance to record a single frame instead of multiple frames?
    I would be very happy if you could help with this.

    0
    Comment actions Permalink

Please sign in to leave a comment.