RealSense Support

What D camera will produce 256 greyscale still photos for a CNC router

Comments

5 comments

  • MartyX Grover

    Hi Ccoker2  If you need to generate 8-bit (256) grayscale images then any of the 400 Series camera models (D415, D435/i, D455) can produce a pair of left and right Y8 (infrared) format grayscale images.  This can be accomplished with the pre-made RealSense Viewer software tool that can export the left and right Y8 frames as PNG image snapshots.

     

     

    By default the Viewer tool overlays its Y8 images with a dot pattern projection, though this can be removed by turning off the camera's IR Emitter in the Viewer's control panel.  A PNG saved from the Viewer will therefore not have the dot pattern overlaid on them, making the image resemble grayscale RGB.  A set of left and right IR Y8 images of a scene is shown below

     

    0
    Comment actions Permalink
  • Ccoker2
    I am not sure I completely understand or follow your answer without further reading.  Attached is an example of what I am targeting.  The file is a 3D rendering in jpeg or bmp.  I am then able to import this into Vetric Aspire and it will become a 3D rendering that I can cut. 
    0
    Comment actions Permalink
  • MartyG

    Apologies if I misunderstood.  "3D photo" suggests a three-dimensional image created by aligning a pair of left and right images to create a view like the combined one created by the left and right eyes.  The image that you have kindly provided above looks like a single infrared image of a three-dimensional object (a hand in this case).

    The Vectric Aspire support page in the link below states that it supports PNG image import, so you may still be able to use the pre-made RealSense Viewer tool to create the image file.

    https://support.vectric.com/aspire-questions/item/can-i-work-image-files  

    There is also a tutorial in the YouTube link below for using Vectric Aspire to make a CNC cut from a PNG image.

    https://www.youtube.com/watch?v=29b0QdNxiQc

    0
    Comment actions Permalink
  • Ccoker2

    It is actually a bmp depth map called my many names that I am finding in the research.  Attached is a link to show how to import and it into Aspire and it will take on the shape of the image.  I have used in only two formats so far; bmp an jpeg.

    https://www.youtube.com/watch?v=LQt-jtpUbY0

     

    0
    Comment actions Permalink
  • MartyX Grover

    You may be able to capture a depth map similar to the above in the Viewer using the White to Black color setting to render the color shading in monochrome.  It would still have to be saved as a PNG though.  It is also worth noting that most of the depth information is lost when saving to PNG file.

     

    0
    Comment actions Permalink

Please sign in to leave a comment.