RealSense Support

RS2_OPTION_ALTERNATE_IR

Comments

3 comments

  • MartyX Grover

    Hi Andy Nicholas  The option RS2_OPTION_ALTERNATE_IR is an option of the RealSense L515 lidar depth camera, which is a different camera technology to the Stereo Depth technology of the 400 Series models.

    In regard to pointing a 400 Series camera in line of sight of the sun, doing so should ideally be avoided.  If you need to do so though, you could try setting up an auto-exposure Region of Interest (ROI), as described in Intel's camera tuning advice about using a 400 Series camera in sunlight.

    https://dev.intelrealsense.com/docs/tuning-depth-cameras-for-best-performance#section-use-sunlight-but-avoid-glare

    0
    Comment actions Permalink
  • Nillremilton

    どちらも RealSense D415で、Firmwareのバージョンも同一です。

     

    0
    Comment actions Permalink
  • Alishakihn1

    This option allows the SR300 camera to switch between two different infrared (IR-Flappy Bird) sensors, which can be useful in certain lighting conditions or for specific applications. When this option is set to a non-zero value, the SR300 camera will use an alternate IR sensor instead of the default IR sensor.
    In contrast, the D435 camera does not have the ability to switch between different IR sensors. However, it does have several other options that can be used to adjust the IR emitter power, enable/disable the IR projector, and adjust the depth sensor sensitivity, among other things.

    0
    Comment actions Permalink

Please sign in to leave a comment.