Supported Win10 version detail for F455/F450
Hello community folks,
This is 1st time for me to post in this community.
Also, I just started to learn about RealSense products.
It will be great if someone can advise me on the following question.
My potential customer is interested in F455/F450.
His question is "Can F455/F450 work with Win10 IoT Enterprise 2019?".
I searched documents for F455/F450 and this community, but I could not find the answer after some amount of effort to find.
Then I found that RealSense ID SDK is tested on Win10 + Visual Studio 2019.
https://github.com/IntelRealSense/RealSenseID/releases
Is this mean that any variant of Win10 should work?
Also, is there a requirement for the PC spec, such as intel processor speed, ram memory, etc?
Thank you,
Kunio Horie
-
Hello Kunio Horie,
It should work fine with Win10 IoT Enterprise but it may not have been explicitly tested with 2019 version. We recommend for the customer test with the target OS.
RealSenseID was designed to work with a wide variety of devices, from low-power single-board computers (SBC) like Raspberry Pi to anything above that. As long as the host has a USB 2 port and runs one of the supported OSes it shoud work. The Tech Specs in the RealSense ID page have more information on the interface and power requirements and the datasheet is also helpful.
Sincerely,
Jesus G.
Intel Customer Support
Please sign in to leave a comment.
Comments
3 comments