RealSense Support

Getting started hosting an F455 on Raspberry Pi 4

Comments

47 comments

  • Yu-Chern Peh

    Hi Ualtboum,

    Check out the Instruction for Linux. After building, you will get a command-line tool to use RealSenseID. 
    Furthermore, there is also a whitepaper about Code Samples for Intel RealSense ID Solution. 


    Regards,
    Yu-Chern​​
    Intel RealSense Customer Support

    0
    Comment actions Permalink
  • Ualtboum

     

    Thank ,

    Thanks for the links  .

    1.Do you have instructions for   how to compile it on  Raspberry Pi 4(the instructions are for Ubunto 18.4)? Do you officially support it ?was it tested?

    2.Is python supported in the Real sense id API? (since in the link below it said that python and java are under dev)

     

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Ualtboum,

    1. The Instruction for Linux is working fine for Raspberry Pi. I've tested it on my side. 

    2. Currently, Python API is still under development and will be supported in later release.

     

    Regards,
    Yu-Chern​​
    Intel RealSense Customer Support

    0
    Comment actions Permalink
  • Ualtboum

    Hi ,

    i followed the instructions on resbery pi  - but it is missing some details:

    it wrote

    > cmake ..
    > make


    the above promts an error
    can you tell me what to put instead of ...
    and the full make command .
    IT WOULD BE REAL HELPFUL TO SUBMIT A REAL FULL COMMAND LINE
    THANKS

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Ualtboum,

    The full make command is cmake .. This ".." is required. After cloning the RealSenseID repository, did you direct to that folder to create a folder named build?

    git clone https://github.com/IntelRealSense/RealSenseID.git
    cd RealSenseID
    mkdir build
    cd build
    cmake ..
    make

    Regards,
    Yu-Chern​​
    Intel RealSense Customer Support

    0
    Comment actions Permalink
  • Ualtboum

    Many thanks I managed to compile it  with your great help .

    in windows I opened the big project in vs2019 and ran the sample authenticate-cpp-sample and it worked great .

    In PI-4  I am a bit confused since I do not see solutions created .

    I ran the command cmake -DRSID_SAMPLES=1 ..

    it worked and placed some files in my build folder but from there I do not know how to continue .

    can you send me some instructions how can I run the authenticate-cpp-sample ?  

     

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Ualtboum,

    After building, you will find the authenticate-cpp-sample in /build/bin directory. Then you can run it with the command: 
    ./authenticate-cpp-sample


    Regards,
    Yu-Chern​​
    Intel RealSense Customer Support

    0
    Comment actions Permalink
  • Ualtboum

    Hello ,

    Thanks for you help I fell we are progressing  .

    I managed to run the auth program but it returns errors allthough I connected the camera via usb:

    ./authenticate-cpp-sample

      [2021-05-30 15:46:44.284] [debug] [LinuxSerial] Opening serial port /dev/ttyACM0 baudrate 115200
    [2021-05-30 15:46:44.285] [error] [FaceAuthenticatorImpl] Failed open serial port. errno: 2
    Failed connecting with status Error
    [2021-05-30 15:46:44.285] [debug] [NonSecureSession] Close session
    program 

     

    I tried to follow up with this command to see what port it is connected but it returned nothing:

    pi@raspberrypi:~/Uri/Intel/clone/RealSenseID/build/bin $ sudo dmesg | grep 'Intel F450' -A 5 | grep ttyACM
    pi@raspberrypi:~/Uri/Intel/clone/RealSenseID/build/bin $

     

    Please tell me what steps I should follow to get the connected usb port name and activate the auth app  .

     

    Many thanks

     

     

     

    0
    Comment actions Permalink
  • Ualtboum

    Hello ,

    Thanks for you help I feel  we are progressing  .

    I managed to run the auth program but it returns errors allthough I connected the camera via usb:

    ./authenticate-cpp-sample

      [2021-05-30 15:46:44.284] [debug] [LinuxSerial] Opening serial port /dev/ttyACM0 baudrate 115200
    [2021-05-30 15:46:44.285] [error] [FaceAuthenticatorImpl] Failed open serial port. errno: 2
    Failed connecting with status Error
    [2021-05-30 15:46:44.285] [debug] [NonSecureSession] Close session
    program 

     

    I tried to follow up with this command to see what port it is connected but it returned nothing:

    pi@raspberrypi:~/Uri/Intel/clone/RealSenseID/build/bin $ sudo dmesg | grep 'Intel F450' -A 5 | grep ttyACM
    pi@raspberrypi:~/Uri/Intel/clone/RealSenseID/build/bin $

     

    Please tell me what steps I should follow to get the connected usb port name and activate the auth app  .

     

    Many thanks

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Ualtboum,

     

    You're using the correct command to get the connected USB port name and the output should have something. Please try to connect the cable with another port of Raspberry Pi. Perhaps you can try to run this 'lsusb' command to make sure your F455 Camera is connected to the Raspberry Pi.

     

     

    Regards,
    Yu-Chern 
    Intel Customer Support

    0
    Comment actions Permalink
  • Ualtboum

    Hi  ,

    I ran the command lsusb and it returned:

    root@raspberrypi:/home/pi/Uri/Intel/clone5# lsusb
    Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
    Bus 001 Device 002: ID 2109:3431 VIA Labs, Inc. Hub
    Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
    root@raspberrypi:/home/pi/Uri/Intel/clone5#

     

    the same results was if the camera is connected or not  .

    I set up a team view on the PI-4  . 

    1 547 193 735

    a123456

     

    please try to login to assist us since we wish to push with the integration - we want to make a demo very shortly in our partners meeting.

    thanks

     

     

    0
    Comment actions Permalink
  • Ualtboum

    I moved it to all other usb ports and the command:

    sudo dmesg | grep 'Intel F450' -A 5 | grep ttyACM

    did not repond....

    I ran the command lsusb and it returned:

    root@raspberrypi:/home/pi/Uri/Intel/clone5# lsusb
    Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
    Bus 001 Device 002: ID 2109:3431 VIA Labs, Inc. Hub
    Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
    root@raspberrypi:/home/pi/Uri/Intel/clone5#

     

    the same results was if the camera is connected or not  .

    I set up a team view on the PI-4  . 

    1 547 193 735

    a123456

     

    please try to login to assist us since we wish to push with the integration - we want to make a demo very shortly in our partners meeting.

    thanks

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Ualtboum,

    It seems like your F455 camera is not detected. Before that, try to connect your F455 camera to a Windows 10 host machine and run with the Intel Realsense ID Viewer. You may also check your F455 camera with the Device Manager.

     

    You have to install the Intel RealSense ID Viewer and Firmware.

     

     

    Regards,
    Yu-Chern 
    Intel Customer Support

    0
    Comment actions Permalink
  • Ualtboum

    Hi ,

    camera was tested and working great with windows  .

    the problem is only with PI .

    please suggest how to proceed?

     

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Ualtboum,

    Glad to know your F455 camera is working fine. The problem now is your F455 camera didn't detect by your Raspberry Pi. You can try to connect them using a powered USB 3.0 hub. Please note that USB 2.0 port is unable to detect F455 camera. 


    Regards,
    Yu-Chern 
    Intel Customer Support

    0
    Comment actions Permalink
  • Ualtboum

    Hi ,

    I got it all to work last week .

    this week this is what I am getting in PI-4  - I cann't get it to work allthough I restarted many times .

    RealSenseID::AuthenticateStatus::SerialError

    [2021-06-13 17:47:28.036] [error] [PacketSender] Failed sending face entry command
    [2021-06-13 17:47:28.036] [error] [NonSecureSession] Failed to send start session packet
    [2021-06-13 17:47:28.036] [error] [FaceAuthenticatorImpl] Session start failed with status 102
    [2021-06-13 17:47:28.136] [debug] [NonSecureSession] Start session
    [2021-06-13 17:47:28.137] [error] [LinuxSerial] Error while sending 16 bytes. errno=5, sent so far: 0, write rv=4294967295

     

    please advise.

    thanks

     

     

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Ualtboum,

     

    The error sounds like it could be a power issue. Have a try with another USB powered cable. Someone has shared his finding regarding similar issue.

     

     

    Regards,
    Yu-Chern 
    Intel Customer Support

    0
    Comment actions Permalink
  • Ualtboum

    Thank you we got it to work and we recieve the events in callback and handle them in our software!!!

    we have 4  issues we would like to address to finish the integration:

    1 . can we connect more than one camera to a PI?

    2. do you also support PI-3? 

    3.in windows we have the intel software that we can capture a face and assign it to authentication . is there a similar software that can be executed in the PI? if so some instructions would be great

    4.I manage to compile the code using visual code on PI with the CMake extension . the problem is that the resulting file

    ./authenticate-cpp-sample   when copied to a diffrent machine results in "fragmentation error" when exectuted . 

    Is there a need to copy addidional files to the same folder of

    ./authenticate-cpp-sample   ?  or some guide to compilations in release mode?...

    Thanks!!!!

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Ualtboum,

     

    1. Can you describe your use case for using multiple F455 cameras?

     

    2. The Instruction for Linux is also working fine for Raspberry Pi 3. I've tested it on my side with a powered USB 3.0 hub. Please note that USB 2.0 port is unable to detect F455 camera. 

     

    3. After building the solution, you will find a rsid-cli in the /build/bin directory. This rsid-cli has the similar functionality as the rsid-viewer in Windows 10, which allows you to enroll and authenticate. The difference is this rsid-cli is a command-line interface, which means don't have the preview frame. 

     

    4. The default build type for the CMake is already in Release mode. But if you compile the code with Visual Code on Pi,  there is an option in the Visual Code interface for you to change Debug to Release. When copying the authenticate-cpp-sample to another machine (Raspberry Pi to another Raspberry Pi), you have to copy also the shared library which is the librsid.so (located in /build/lib directory) and paste it into /lib directory.

     

     

    Regards,
    Yu-Chern 
    Intel Customer Support

    0
    Comment actions Permalink
  • Ualtboum

    Thanks you are very helpful!!

    1. Can you describe your use case for using multiple F455 cameras?

    we would like to connect several cameras to one PI and run a few of our application each listening for callbacks from an SDK on a diffrent camera on a diffrent usb port 

    Is the above possible ?

     

    0
    Comment actions Permalink
  • Ualtboum

    Hello ,

    I wish to tell us what we wish to achieve and maybe you'll have some ideas .

    We wish to use one windows main station to delare the users with the nice windows interface .

    than we would like to take the photo and the names from the camera and share it with many more resbery PIs 1...n

    we do not want to do every declaration per each PI we would like some kind of way/sdk to update all  selected PIs from the main station .

     

    Can you please suggest how to apply the above?

    than we would like to upload the selected image 

    0
    Comment actions Permalink
  • Ualtboum

    Hello ,

    I wish to tell us what we wish to achieve and maybe you'll have some ideas .

    We wish to use one windows main station to delare the users with the nice windows interface .

    than we would like to take the photo and the names from the camera and share it with many more resbery PIs 1...n

    we do not want to do every declaration per each PI we would like some kind of way/sdk to update all  selected PIs from the main station .

     

    Can you please suggest how to apply the above?

    than we would like to upload the selected image 

     
    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Ualtboum,

    There are device mode and host mode in the RealSense ID Viewer.

    Device Mode is a set of APIs enable the user to enroll and authenticate on the device itself, including database management and matching on the device.

    Host Mode is a set of APIs for users who wish to manage a faceprints database
    on the host or the server.

    Enroll the users in host mode of RealSense ID Viewer. The database will save in a .db file. If you save the .db file in default path, you can find this .db file in this way: Right-click the Intel RealSense ID Viewer and then select "open file location".

    After done enroll, change the mode to device mode (which is 'Host mode: No' in the setting). You can save the database to the device by importing this .db file. It is a good practice to click the "store updates to flash" button although the system will auto-update after importing the .db file.

    You may refer to the link below for a better picture.
    https://www.intelrealsense.com/get-started-intel-realsense-id/


    Regards,
    Yu-Chern 
    Intel Customer Support

    0
    Comment actions Permalink
  • Ualtboum

    Hello ,

    thanks for the response .

    sorry I did not really understand how to accompilish what we need.

    we have a dedicated windows machine there we will declare the user on the realsense camera connected to this pc .

    we have 1..n resbery PI connected in the network  . and now we want to update them all with the picture delared on our windows machine . 

     

    How do we do that ?

    Can you send us specific documents protocols to implement?

    many thanks

     

    0
    Comment actions Permalink
  • Ualtboum

    Hi ,

    what we mostly do not understand is after we have configured it in host mode and have the db file .

    now we have 300 cameras - how can we  deploy this file to 300 cameras programmingly? 

    is there an sdk ? 

    or do we have to manually copy the file to each camera and make manual operations for it to load the db created in the host?

    If there are some documents/code sample  about updating the cameras with the db it would be great  .

    thanks

     

    0
    Comment actions Permalink
  • Ualtboum

    Hello  ,

    I managed to create the db file using host mode  .I have several open questions I would thank you if you could answer:

    1. I noticed there is an export option and an import option (JSON) .  - so why do we need the db file ?(since we can import and export using the json format)

     

    2.  I need a c/C++ sample of how to upload the json or the db (created by the host) to a camera . Can you please send me ?

     

    Thanks

     

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Ualtboum,

    I apologize for the previously proposed solution which is importing the db file from the host to the device. There is a robust way without importing the db file manually. 

    In Host mode, the faceprints database (db) file is stored outside of the RealSense ID, on a central PC so that all of the Raspberry Pis can access the faceprints db over a network. Use the server mode APIs ExtractFaceprintsForEnroll, ExtractFaceprintsForAuth, and MatchFaceprints. Refer to host_mode.cc for an example of how to use the host mode APIs.

    Enrollment Flow
    1.Person enrolls on RealSenseID connected to a device of choice.
    2. The device extracts the faceprint from the RealSenseID, using ExtractFaceprintsForEnroll, and saves the faceprint to the faceprints database which is stored in a central location, such as a PC.

    Authenication Flow
    1.Person authenticates on RealSenseID connected to device of choice. The device must have access to the central location where the faceprints db is stored.
    2. The device extracts the faceprint from the RealSenseID using ExtractFaceprintsForAuth.
    3. The device calls MatchFaceprints to compare user faceprint to faceprints in the centralized faceprints db.

    The attached picture shows the flow graphically.

    0
    Comment actions Permalink
  • Ualtboum

    Hello ,

    thanks for the information .

    I tried to figure it out but it is too complex . I looked for a place to specify the ip address of the remote pc central station and could not find any sample showing the remote clients connecting to host and checking the face  .

    can you please try to assist:

    1 . is the  host_mode.cc   suppose to run on the client (PI in our case) or the central pc station?

    2. Where is the sample running on the other side?

    in other words we need a client code and a server code and some example how to connect between them .

    any information would be appreciated to overcome the confusion .

    Many thanks for your help .

     

    0
    Comment actions Permalink
  • Ualtboum

    to make my question a bit more clear : 

    I noticed that this code should run on our PI and connect some how to the main station to get the auth   .

    In the following code I do not see and connection details such as IP address of the host central pc so I do not understand how to connect to it . Is there a full code example showing both the server and the client side?

    // extract faceprints using enrollment flow
    class MyEnrollServerClbk : public RealSenseID::EnrollmentCallback
    {
        const char* _user_id = nullptr;
    
    public:
        explicit MyEnrollServerClbk(const char* user_id) : _user_id {user_id}
        {        
        }
    
        void OnResult(const RealSenseID::EnrollStatus status, const Faceprints* faceprints) override
        {
            std::cout << "result: " << status << "for user: " << _user_id << std::endl;
            s_extraction_status = status;    
            // if status was success pass '_faceprints' to user            
        }
    
        void OnProgress(const RealSenseID::FacePose pose) override
        {
            std::cout << "pose: " << pose << std::endl;
        }
    
        void OnHint(const RealSenseID::EnrollStatus hint) override
        {
            std::cout << "hint: " << hint << std::endl;
        }
    };
    
    MyEnrollServerClbk enroll_clbk {user_id.c_str()};
    auto status = authenticator->ExtractFaceprintsForEnroll(enroll_clbk);


    0
    Comment actions Permalink
  • Ualtboum

    Hello ,

    we are interested in the solution of exporting the host db file to all PIs .

    we asked a couple days ago the following  and we would thank you if you can respond since we need to proceed with this project .

    How can we import the db file to the resberry PI?

    is there an API  sdk funtion that loads imports it?or should it be placed on a specific directory?

    please advice.

    thanks

     

     

    0
    Comment actions Permalink

Please sign in to leave a comment.