RealSense Support

example.hpp: No such file or directory

Comments

5 comments

  • MartyX Grover

    Hi Blake58  Could you check please whether there are pre-built and ready to execute versions of the librealsense examples in the Ubuntu folder usr/local/bin

    If the pre-built examples are present then you should be able to run them from the Ubuntu terminal.  Could you try inputting rs-capture into the terminal.  You should also be able to launch the RealSense Viewer from the terminal by inputting realsense-viewer

    0
    Comment actions Permalink
  • Blake58

    Hi MartyG Thanks for help me. There are any files in my bin folder

    but, in terminal, if i run 'rs-capture', then the code runs perfectly,

    but, we want to get only depth image, so we tried to custom rs-capture code in qt creator, but in qt, we cant run code.

    what we want to do is get realtime depth image by d435 and use it at jupyter notebook. Does it impossible?

    0
    Comment actions Permalink
  • MartyX Grover

    There is a Jupyter Notebook example called depth_filters that could act as the basis for such a project.  It accesses depth data from a recorded bag file and applies post-processing filters to the depth.

    https://github.com/IntelRealSense/librealsense/blob/jupyter/notebooks/depth_filters.ipynb

    Just as live camera example programs can be adapted for use with bags, I would speculate that the reverse is also true and that the Jupyter notebook example could be adapted to use a live camera pipeline.  For example, taking the line cfg.enable_device_from_file("stairs.bag")

     

     

    And replacing it with:

    cfg.enable_stream(rs.stream.depth, 640, 480, rs.format.z16, 30)

    0
    Comment actions Permalink
  • Blake58

    Finally we can use d435 in our jupyter. Because of my bad english, i don't know how to express our mood.

    Thanks you so much for dealing our one month delayed project. I think we can pass our graduate exam. Thank you so much again

    0
    Comment actions Permalink
  • MartyX Grover

    You are very welcome.  I am pleased that I could help.  Good luck with your project and exam!

    0
    Comment actions Permalink

Please sign in to leave a comment.