3D scan of an instrument
Hello,
since this morning I'm dealing with an Intel RealSense Depth Camera D455 with which I should acquire a 3D scan of an instrument, to be imported later in Autodesk Inventor. Based on the information and examples of use that I have found so far and on the first tests I have done, it seems that this camera is suitable for making a 3D scan of relatively large objects such as a car, while it's not possible to reach the resolution necessary to draw a fairly accurate scan of the instrument in question, which has small parts such as buttons. Am I wrong? Do you have any suggestions for me?
Thanks in advance, and best regards!
Alessia
-
Hi Alessia Lamanna If you are aiming to import a scan into Autodesk Inventor then it sounds as though you are trying to create a solid 3D model scan such an .obj or .dae file. Is that correct please? If so, one of the available methods for accomplishing this would be to create a point cloud scan of the object in the free RealSense Viewer tool and then export the scan as a .ply file and import the ply into a 3D modelling software package that supports ply import (either by default or with a plugin).
The link below has a tutorial for creating a point-cloud ply in the RealSense Viewer and then importing it into a free tool called MeshLab for conversion to a solid mesh in a file format such as .obj or .dae.
https://www.andreasjakl.com/capturing-3d-point-cloud-intel-realsense-converting-mesh-meshlab/
As mentioned above, a ply can also be imported into other 3D modelling software, such as Blender and Maya.
If you are performing close-range scanning with the RealSense Viewer of a small object then the discussion in the link below about enhancing image quality when scanning a toothpick may be helpful.
https://github.com/IntelRealSense/librealsense/issues/8228
There are also RealSense-compatible commercial 3D scanning solutions available. If you have access to Windows or Android, DotProduct Dot3D Scan is compatible with the D455 camera model and has a free trial version.
Please sign in to leave a comment.
Comments
1 comment