View my account

D455-How can I see far away

Comments

1 comment

  • MartyX Grover

    Hi N Kanbe I9  If you are using the RealSense Viewer tool and your depth range is limited to 4 meters then it may be because a post-processing filter setting called the Threshold Filter is enabled. This limits the depth data rendered to values up to a maximum of 4 meters by default.

    The status of the Threshold Filter can be checked in the Viewer in the options side-panel.  Expand open the Stereo Module options and then expand the Post-Processing sub-category.  Look for the Threshold Filter option in the list of filters.  If it has a blue icon beside it (which indicates that it is On), left-click on the blue icon to turn it to red (Off).    The camera should then be able to render on the depth image the full distance range of depth data that it is able to observe.

     

    0
    Comment actions Permalink

Please sign in to leave a comment.