View my account

Memory leak when using context.QueryDevices (C # D455)

Comments

6 comments

  • MartyX Grover

    Hi Shimamoto1991  When the memory is leaking, do you experience any memory errors (like in the C# case in the link below) or is it leaking silently with no warnings?

    https://github.com/IntelRealSense/librealsense/issues/8272

    Also, is it possible for you to update your SDK version to a current one such as 2.44.0 to see whether it makes a positive difference, please?

    0
    Comment actions Permalink
  • Shimamoto1991

    Hello, MartyG
    The memory leak is silent without warning.
    Judging from how the process memory of the diagnostic tool of Visual Stdio 2019 goes up.

    I've also updated the firmware and SDK version to the latest version, but I'm still having problems.

    Firmware: ver 5.12.12.100
    SDK: ver 2.44.0.0

    D455

     

    D435

    0
    Comment actions Permalink
  • MartyX Grover

    A C++ user reported a similar memory leak pattern with Visual Studio 2019 in January 2020.  In their report, D435 displayed the same flat constant pattern as your D435, but D435i and D455 had the upward slope.

    https://github.com/IntelRealSense/librealsense/issues/8091#issuecomment-759975908

     

     

    As shown in the report linked to above, the D455 had an extra element in its memory heap snapshot named realsense2.dll__vcrt_ptd that the D435 did not have that was increasing the byte usage considerably.  Does your D455 chart in Visual Studio have this same extra element, please?

     

    0
    Comment actions Permalink
  • Shimamoto1991

    Thank you for the information.
    Looking at the memory usage graph, it seems similar to the problem I'm facing.
    I tried taking a snapshot, but unfortunately it doesn't look the same as above.
    I'm not very familiar with this field, and the heap size etc. hasn't changed in the snapshots I took, so it may just not be taken correctly ...

    By the way, in the similar case you taught me, it seems that it has not been solved as a result.
    Should I consider any other method because my goal is to get RealSense connectivity?

    0
    Comment actions Permalink
  • MartyX Grover

    I believe that in C# the device connection status can be checked with OnDevicesChanged

    https://github.com/IntelRealSense/librealsense/issues/3142#issuecomment-465494716

     

    0
    Comment actions Permalink
  • Shimamoto1991

    OK, I'll give it a try!
    Thank you very much.

    0
    Comment actions Permalink

Please sign in to leave a comment.