RealSense Support

Intel® RealSense™ LiDAR Camera L515

Comments

1 comment

  • Munesh

    Hi Kaveh,
    Thanks for reaching out to us.
    The LiDAR L515 is not a 360-degree LiDAR. It has a FOV of 70° x 55°. You can find more information in the L515 datasheet.
    You can do SLAM with the L515 but you will have to implement your own solution. Intel posted this sample SLAM using D435i but it can be used with the L515 too. 
    You can also refer to SLAM using L515 as an example project created by a 3rd party, not supported by Intel.

    Regards,
    Munesh

    Intel Customer Support

    0
    Comment actions Permalink

Please sign in to leave a comment.