View my account

D435 Depth No frames received

Comments

16 comments

  • MartyX Grover

    Hi Kapitanyv  I have considered your case carefully.  Could you confirm to me please that you are running both Linux and Windows on the same Windows host computer, please?  And if so, are you using Windows Subsystem for Linux (WSL) as the basis of your Linux system?

    Also, is the Windows version of the RealSense Viewer still able to detect the camera and display its details with the 'Info' option at the top of the options side-panel, even if you cannot successfully activate the depth stream?  If it can show these details, and display the correct firmware version, then that would make it less likely that the firmware is the cause of the problem.

    Do you have a different USB port on the computer that you can try the camera in if you have not done so already, please?

    0
    Comment actions Permalink
  • Kapitanyv

    Hi MartyG thanks for responding!

    Both Linux and Windows are running on the same Windows host, yes.

    No I'm not using WSL, I'm using VMWare to run a real virtual machine, and have tried a VM in Virtualbox as well before, but I read on github that Intel recommend to use VMWare instead because it claims better USB emulation  https://github.com/IntelRealSense/librealsense/blob/development/doc/installation.md

    Yep, both the Linux and Windows Realsense Viewers detect the camera, show the RGB stream and show 'info'

    I don't know if it helps, but if I try to update the firmware, it gives me this error message

    I get here by clicking 'update firmware' and selecting a .bin file I downloaded from https://downloadcenter.intel.com/download/30246/Firmware-for-Intel-RealSense-D400-Product-Family. Although, the firmware on the device is v5.12.12.100, so maybe this is only telling me that 'update firmware' cannot downgrade the firmware, only upgrade it.

     

    0
    Comment actions Permalink
  • MartyX Grover

    The camera will prevent downgrade to an older firmware version if such a downgrade has been performed 20 times in the camera's lifetime.  After that, the camera will only permit update to a newer firmware than the one that is currently installed (which is 5.12.12.0 in your case).   The firmware looks okay to me though.

    Next, we will try restoring the calibration of the camera to its factory settings.  Please go to the More option in the Viewer and select Calibration Data from its menu.

    In the box that appears on screen, left-click on the box in the bottom corner labelled I know what I'm doing to highlight it.  Then left-click on the Restore Factory option in the top corner of the box.

    Finally, left-click on Cancel to exit the window and try enabling the depth stream.

    Does this improve the camera's ability to stream depth, please?

     

     

    0
    Comment actions Permalink
  • Kapitanyv

    Hi MartyG,

    It doesn't help.

    0
    Comment actions Permalink
  • MartyX Grover

    Thanks very much for your patience.

    Next, please unplug the micro-size end of the USB cable from the side of the camera, turn it upside down and re-insert it (USB-C cables are two-way insertion on the micro end).

    0
    Comment actions Permalink
  • Kapitanyv

    Hi, that doesn't help either.

    0
    Comment actions Permalink
  • MartyX Grover

    Which method did you use to install the RealSense SDK on Windows, please?  Did you go to the SDK Releases page and use the automated installer file?

    https://github.com/IntelRealSense/librealsense/blob/master/doc/distribution_windows.md#installing-the-sdk

     

    0
    Comment actions Permalink
  • Kapitanyv

    Hi, 

    I first followed the installation instructions for linux, and then when it stopped working on linux and I wanted to test on windows, I installed the SDK via the automated installer, yes.

    0
    Comment actions Permalink
  • MartyX Grover

    There was a recent case on the RealSense GitHub forum involving a VMware virtual machine on Windows that also had No Frames Received (on the RGB stream instead of depth in that case).

    https://github.com/IntelRealSense/librealsense/issues/8651

    The RealSense user in that case found that the camera worked fine on the host but not on the VM, and the highest resolution that they could use successfully on the VM was 640x480 at 30 FPS.  

    0
    Comment actions Permalink
  • Arvind Sonar

    I am having Intel Realsense depth camera D435F using on Win 11 pro on host machine. I am getting same error of No Frame received. How to resolve?

     

    0
    Comment actions Permalink
  • MartyX Grover

    Hi Arvind Sonar  Has your camera been stored unused for a period of weeks / months in a location such as a cupboard or drawer before you tried the camera and experienced the no frames received error, please?

    0
    Comment actions Permalink
  • Arvind Sonar

    Yes, it was in cupboard for long period of time. 

    But When I was installed latest setups on PC having OS widows 10 pro, it was working properly. 

    I am having 3 cameras, all are having same issue. 

    0
    Comment actions Permalink
  • MartyX Grover

    Storing a RealSense camera in a cupboard for a long period can cause a fault in the camera hardware that results in the No Frames Received message on the depth stream shown at the top of this discussion.  It is not known why it occurs but it may be related to the environmental conditions within the storage space.  As it is a hardware issue there is usually no way to recover the camera to working condition, unfortunately.  

     

     

    There was one case where a camera with this condition recovered after being sent through the post, perhaps restored by warmth during transit, but in most cases the only course of action available is to replace the camera.  If the cameras were purchased less than 12 months ago then they will still be under warranty and you could enquire to the retailer they were purchased from about an RMA return for a replacement.

    0
    Comment actions Permalink
  • Arvind Sonar

    Then how this camera is working perfectly on win 10 pro? 

    0
    Comment actions Permalink
  • Arvind Sonar

     

    0
    Comment actions Permalink
  • MartyX Grover

    If the camera is working on Windows 10 Pro then there is fortunately not likely to be a hardware failure caused by storage conditions, otherwise depth would not work on any computer the camera was attached to.

     

    On the Windows 11 Pro computer, please check whether permission to access the camera hardware and permission for applications to use the camera are both set to On in the Windows camera privacy settings using the instructions at the link below.

    https://github.com/realsenseai/librealsense/issues/3381#issuecomment-503424789

    0
    Comment actions Permalink

Please sign in to leave a comment.