Kapitanyv
- Total activity 6
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Activity overview
Latest activity by Kapitanyv-
Kapitanyv commented,
Hi, I first followed the installation instructions for linux, and then when it stopped working on linux and I wanted to test on windows, I installed the SDK via the automated installer, yes.
-
Kapitanyv commented,
Hi, that doesn't help either.
-
Kapitanyv commented,
Hi MartyG, It doesn't help.
-
Kapitanyv commented,
Hi MartyG thanks for responding! Both Linux and Windows are running on the same Windows host, yes. No I'm not using WSL, I'm using VMWare to run a real virtual machine, and have tried a VM in Virtu...
-
Kapitanyv created a post,
D435 Depth No frames received
OS: Ubuntu 20.04 VM (VMWare) on Windows 10 host, as well as the Windows 10 machine SDK: v2.43.0 (Linux), v2.42 & v2.41 (Windows) USB: 3.2 Firmware: 5.12.12.100 (Linux) 5.12.11.00 (Windows) Languag...