RealSense Support

Couldn't Capture Synchronous frames from two Realsense Depth cameras D435i

Comments

14 comments

  • Jesus Garcia

    Hello Sandeep,

    There are several things you can try:

    • Make sure to use the latest FW. There was a bug in older FWs that 6fps sync does not work. Or use a higher frame rate, e.g. 15 fps.
    • Use Master and Slave for the two D435i. Don't use Genlock mode.

    The difference between the two cameras should be less than 1us.

    Sincerely,
    Jesus G.
    Intel Customer Support

    0
    Comment actions Permalink
  • Sandeep Tammana

    Hello Jesus,

    Thank you for your reply.

    Could you please provide your feedback on the below 4 queries:

    Thank you,

    Best Regards,

    Sandeep

    0
    Comment actions Permalink
  • Sandeep Tammana

    Hello Jesus,

    Additional to above 4 points, i missed to mentioned the below point:

    5) We connected two real sense cameras earlier using the external connector Pin 5 (sync) and Pin 9 (GND). One camera is set as master and another as Slave / Full slave. Both were set with 6FPS.

    In this case, the captured images are not in sync . We will try to repeat the same with the higher frame rate. 

    https://dev.intelrealsense.com/docs/multiple-depth-cameras-configuration#section-e-external-trigger  

     

     

    0
    Comment actions Permalink
  • Btasa

    Pin 5 (sync) connected to pin 4 of the slaves. Thats the way you have it wired right? 

     

    0
    Comment actions Permalink
  • Sandeep Tammana

    Hello,

    The connection is as follows:

    Pin 5 (Sync) of master to Pin 5 (Sync) of slaves.

    Pin 9 (GND) of master to Pin 9 (GND) of slaves.

     

     

    0
    Comment actions Permalink
  • Sandeep Tammana

    Hello Jesus,

    Could you please provide your feedback for the above 5 queries.

    Thanks a lot for your support

    Best regards,

    Sandeep

     

    0
    Comment actions Permalink
  • Jesus Garcia

    Hello Sandeep,

    I apologize for missing a very important detail in your first post. It is impossible to sync RGB streams across D435-based cameras because the RGB sensor is physically on a separate board from the depth sensors and the sync pin is not connected to it. On D435/D435i cameras, only depth streams can be synced across multiple cameras.

    You should use the latest version of librealsense.

    Sincerely,
    Jesus G.
    Intel Customer Support

    0
    Comment actions Permalink
  • Sandeep Tammana

    Hello Jesus,

    Thank you for your feedback. 

    Can you please suggest any other possible work around to sync the RGB colour frames for D435/D435i cameras. It is quite important for us in the current stage to sync the RGB streams using the Realsense Depth cameras D435i
    Additionally, Could you please suggest a method to test the sync of depth frames from 2 cams? 
    Is there any other version of D435/D435i cameras where we can sync the colour frames ? 
     
    Thank you for your support,
    Best Regards,
    Sandeep
     
    0
    Comment actions Permalink
  • Sandeep Tammana

    Hello Jesus,

    Could you please let us know if you have any feedback on the above query ?

    Thank you for your support,

    Best Regards,

    Sandeep

    0
    Comment actions Permalink
  • Aznie Syaarriehaah

    Hi Sandeep,
    It is impossible to sync the RGB color frames for D435/D435i camera since the RBG and Depth Sensor are on different PCB. The D435 only has depth sync. There is no other version of the D435/D435i camera that can do that. This is only possible with the D415 camera since the RGB and Depth Sensors are on the same PCB board.

    Regards,
    Aznie
    Intel Customer Support

    0
    Comment actions Permalink
  • Sandeep Tammana

    Hello Aznie,

    Thank you for your feedback.

    Could you please suggest a method to test the sync of depth frames from 2 cams in D435 / D435i ? 
     
    Best Regards,
    Sandeep
    0
    Comment actions Permalink
  • Aznie Syaarriehaah

    Hi Sandeep, 
    You can refer to this article on how to sync the D435 via hardware. Hence, there is a whitepaper on External Synchronization of Intel® RealSense™ Depth cameras that might be helpful to you.

    Regards,
    Aznie
    Intel Customer Support

    0
    Comment actions Permalink
  • Sandeep Tammana

    Hello Aznie,

    Thank you for your feedback. I am sorry if my question is bit confusing. I will try to further elaborate.

    We are clear about the hardware sync procedure (Connecting multiple cameras together and also with external sync) right from the beginning.

    We have gone through the whitepapers multiple times related to the external sync and also have applied the external sync exactly as per the recommendation from the whitepaper. We have also connected two cameras via the external sync connector and have set one as master and other as slave.

    We were actually looking for RGB sync and It is clarified in this thread that the RGB colour sync is not possible with D435 / D435i and only depth sync is possible by connecting multiple cameras.

    My query is that how could we ensure that the depth sync is working after connecting the multiple cameras (by setting one as master and others as slaves)  

    Thank you for your support,

    Best Regards,

    Sandeep

     

     

    0
    Comment actions Permalink
  • Aznie Syaarriehaah

    Hi Sandeep Tammana,
    In section 3 of the Multi-Camera Configuration paper explains:

    Now to the somewhat counterintuitive aspect of time stamps. If NO HW sync is enabled, the timestamps will now surprisingly appear to be perfectly aligned. This is because each individual ASIC is counting the exact same number of cycles between frames, and then sending them off. So according to their own timelines, they are sending frames at say, exactly 33.333ms intervals, for a 30fps mode. By contrast, if HW Sync is enabled, the timestamps will actually drift over time. You might expect this drift to be on the order of less than 1ms/minute. Knowing this, you can actually validate that your sync is working by looking at the drift in the difference of the timestamps. If you see NO DRIFT, then there is NO HW sync. If you see DRIFT, then the units are actually HW synced.

    Regards,
    Aznie
    Intel RealSense Customer Support

    0
    Comment actions Permalink

Please sign in to leave a comment.