RealSense Support

LIDAR 515 "industrial" version for high temp environments

Comments

1 comment

  • Official comment
    Jesus Garcia

    Hello Davide,

    The L515 must be kept within those operating parameters in order to maintain depth performance. We do not have a recommended solution to extend the temperature range. If the ambient temperature goes beyond 30° then you should build a housing for the camera that cools it down to a more appropriate temperature. The housing should not block the air vents around the perimeter of the camera and should not place any material, i.e. glass, plastic, etc, in front of the sensors.

    Sincerely,
    Jesus G.
    Intel Customer Support

    Comment actions Permalink

Please sign in to leave a comment.