RealSense Support

Which RealSense product is right for me? D455 or L515?

Comments

5 comments

  • Official comment
    Jesus Garcia

    Hello Michael,

    Update: I just noticed you want HD depth resolution. The L515 does not offer 1280x720 depth resolution. The highest depth resolution available for the L515 is 1024x768.

    The D455 offers 1280x720 depth resolution.

    I recommend you read this paper before you decide: https://www.intelrealsense.com/which-device-is-right-for-you/

    Both cameras may work for you. The L515 is very sensitive to ambient light so it works better with less light. If lighting is minimal, then the L515 may give you better fidelity at those distances.

    I recommend purchasing a couple of units of each type of camera and testing them. The code-base is the same.

    Sincerely,
    Jesus G.
    Intel Customer Support

    Comment actions Permalink
  • Michael Davey

    @... any guidance, please?

    0
    Comment actions Permalink
  • Michael Davey

    @... many thanks for your reply.

    We want to use the camera in an environment where we are controlling the lighting.  We are using a mixture of LED and fluorescent lighting - the area will be well lit but we can carefully grade the lighting to minimise the presence of light sources at 860nm by placing IR cut-off filters over each light source.  There won't be any natural light on the scene.

    Am I correct in thinking that the L515 sensor is very sensitive to light at 860nm but any light hitting the sensor that is from the visible band or UV frequencies, shouldn't cause any problems?

    0
    Comment actions Permalink
  • Jesus Garcia

    Hello Michael,

    You should be okay under those controlled light conditions. Again, text extensively.

    Sincerely,
    Jesus G.
    Intel Customer Support

    0
    Comment actions Permalink
  • Michael Davey

    Thanks for the prompt reply Jesus, much appreciated!

    0
    Comment actions Permalink

Please sign in to leave a comment.