lost connection to one of four d435 cameras
We connect four d435 camera to a four ports of PC using four USB3.0 cables
and camera setting is:
color frame: 640*480@15fps
depth frame: 480*270@15fps
depth aligned to color
one of the four camera lost connection when they are working(cameras are located on a cart) ,
there is no connection information in /proc/bus/input/devices
any advice or solution for us?
-
Hi Lixuefeng Is the disconnection a one time only event or has it occurred repeatedly, please?
-
MartyG it occured frequently, every two or three days
-
Thank you. Are you performing a long-run session with the cameras continuously over a period of days? If so, the 400 Series cameras should be able to run indefinitely if they remain within recommended temperature tolerances. If a problem does occur during a multi-day long run session and the camera has not experienced excessive temperature, it is typically related to a non-camera problem such as the USB equipment (cable or hub), the computer hardware or the computer's operating system.
Please sign in to leave a comment.
Comments
3 comments