There are no connected devices(L515)
I could not find any information for this problem.
What do i need to do next ?


-
I didn't do anything wrong. I have two L515 camera. and my colleague also using two L515. The faulty camera was not connected well before like usb2.0 even i connected with usb3.0. I contacted to reseller in korea. they said if it passed one year after buy the camera. they can not do any service.
I Firmware Updated with SDK 2.35.2. after Firmware Update the camera not working.
I don't think so it's my fault the reason of a faulty camera

Please sign in to leave a comment.
Comments
2 comments