RealSense Support

Make D415 left and right infrared image brighter.

Comments

5 comments

  • MartyG

    Hi Yixun Liu  The infrared image will brighten if the Laser Power setting's value is increased from its default value of '150' to its maximum value of '360'.  Python code for setting Laser Power can be found at the link below.

    https://github.com/IntelRealSense/librealsense/issues/1258#issuecomment-374112555

     

    The infrared option can also be brightened by increasing gain, though as you mention, setting a manual exposure or gain value automatically disables auto-exposure.  So if you wish to keep auto-exposure enabled, increasing Laser Power may be the most appropriate action.

     

    RS2_OPTION_DIGITAL_GAIN does not control gain on 400 Series cameras.  It is a setting on the L515 camera model.  Use RS.OPTION.GAIN instead.  There is not an example script for doing so, though you should be able to set gain if you use the Python code for exposure - sensor.set_option(rs.option.exposure - at the link below and change 'exposure' to 'gain'.

    https://github.com/IntelRealSense/librealsense/issues/4449#issuecomment-514226669

     

    You can use RS.OPTION.CONTRAST to set the contrast, though as contrast is an RGB option rather than a depth option you should access the RGB sensor instead of the depth sensor.  you can do this by setting a sensor index number of '1' (as '0' is the depth sensor) using the query_sensors() instruction, like in the Python script here:

    https://github.com/IntelRealSense/librealsense/issues/10143#issuecomment-1013340798

     

    But as Contrast is an RGB option, changing it will have no effect on the Infrared brightness.

    0
    Comment actions Permalink
  • Yixun Liu

    I just want to double check is the RS2_OPTION_GAIN used for the infrared sensor.?

    From rs_option.h, it looks it is used for the color sensor.

    RS2_OPTION_GAIN, /**< Color image gain*/

    0
    Comment actions Permalink
  • MartyG

    Both depth / infrared and RGB have a gain option.  By default RS2_OPTION_GAIN will affect depth / infrared.  To change RGB gain, the program has to be told specifically to access the RGB sensor.

     

    When gain is increased above its default value of '16', it makes the depth image noisier and increases the brightness of the infrared image. 

    0
    Comment actions Permalink
  • Yixun Liu

    If I want to increase the brightness with auto exposure on I can change the "mean intensity set point" value. Does this require the advanced API? I need to build it by myself, right?

    0
    Comment actions Permalink
  • MartyG

    Yes, the Mean Intensity Setpoint is an Advanced Mode setting.  Code for defining the setpoint can be found at the link below.

    https://support.intelrealsense.com/hc/en-us/community/posts/12316079216147-Set-mean-intensity-value-for-AE-for-D415

     

    Support for Advanced Mode is not something that you need to build.  It is enabled by default in RealSense 400 Series cameras.

    0
    Comment actions Permalink

Please sign in to leave a comment.