RealSense Support

Module D430 without RGB sensor

Comments

18 comments

  • MartyG

    Hi Roman Leuzinger  The D430 is a caseless Depth Module that is not equipped with an RGB sensor.  When the D430 is used in the cased RealSense D435 and D435i models, the RGB sensor is connected separately via a cable.

     

    A D430 Depth Module must be combined with a Vision Processor D4 Board and an interposer to connect the two together, which can be a flexible custom-made cable or a rigid circuit board that can be purchased pre-made.

     

     

    You could explore the possibility of using a Chameleon XS commercial enclosure product for RealSense D415, D435 and D455 USB cameras that has IP66 and IP67 protection.  It may be possible to place the D435 version of the housing around a D435f as the two models have almost the same physical measurements (90 mm × 25.8 mm × 25 mm for D435f, and 90 mm × 25 mm × 25 mm for D435).

    https://www.autovimation.com/en/enclosures-en/chameleon-xs-realsense-en

    0
    Comment actions Permalink
  • MartyG

    In regard to modules with an RGB sensor, the D415 model of Depth Module has an integrated RGB sensor on its PCB. 

     

    The D401 Depth Module has RGB without an RGB sensor, as it can output high quality RGB from its depth sensor without needing a separate RGB component, though D401 is designed for short range (ideal depth sensing range 7 cm to 50 cm).

    0
    Comment actions Permalink
  • Roman Leuzinger

    Thanks for the feedback.

    Unfortunatelly the proposed case from Autovimation is too big for our application. Otherwise it would be the ideal solution. Probably we do have not other joice as to build our own casing. Either integrating the D435F completely or just its modules.

    Do you sell as well the RGB sensor standalone?

    Does the D4 Board integrate an interface including connector towards an external RGB sensor?

    0
    Comment actions Permalink
  • Roman Leuzinger

    In fact RGB is not really required. What we need is an additional camera.

    The setup which I think about is:

    - Covering the 2 stereo cameras with IR filter

    - Having a 3rd camera without IR filter. This camera is only used to read a 2D code (black/white) which is illuminated by robot LED spotlights

     

    Backup would be:

    Using D430 with IR filter. Implementing an external IR illumination which is just activated when we want to read the 2D code. Reading than the 2D code with one of the stereo cameras.

    0
    Comment actions Permalink
  • MartyG

    The RGB sensor is not sold standalone, though it is my understanding from previous discussions on the subject that sensor modules that meet the MIPI CS-2 interface format should be compatible.

     

    Regarding connecting an RGB sensor to the D4 Board, the link below should be a useful reference.

    https://github.com/IntelRealSense/librealsense/issues/1362

     

    The D435f's CLAREX NIR-75N filter is available for purchase separately, opening the possibility of fitting it over the sensors of another RealSense cased camera or caseless Depth Module.  More information can be found here:

    https://astraproducts.com/info-acrylic-nir-filters.asp

    0
    Comment actions Permalink
  • Roman Leuzinger

    Could you give me some more information about the mentioned interposer which can be a rigid circuit board that can be purchased pre-made?
    - Manufacturer
    - Produt name and number

    It would be interesseting if there exist as well a buyable flex cable fitting the needs to contact the two boards. If that should not fit in our design, we still can make one specific to our needs.

    0
    Comment actions Permalink
  • MartyG

    A custom flex interposer cable can be ordered from the company listed below, which is the officially listed supplier in the RealSense 400 Series data sheet document.

     

    Cocom Consumer Electronics Ltd

    Name: Janine Langdale
    Office phone: +44 (0) 1444 461620
    Mobile phone: +44 (0) 7905 692131

    0
    Comment actions Permalink
  • MartyG

    Filters will not let me post the contact email address so I will break it down into plain text so you can reassemble the address.

    Janine.Langdale

    AT

    cc-e dot co dot uk

    0
    Comment actions Permalink
  • MartyG

    The rigid interposer PCB board can be purchased from component suppliers such as FRAMOS, Mouser and Rutronik24.

     

    https://www.framos.com/en/products/d400-rigid-50-pin-interposer-20737

    https://eu.mouser.com/ProductDetail/Intel/82635DSITR50P?qs=wd5RIQLrsJhIJqpBcxiaKQ%3D%3D

    https://www.rutronik24.com/product/intel/82635dsitr50p/9745177.html

     

    Manufacturer: Intel

    Product Name: Intel RealSense D400 Rigid 50 Pin Interposer

    Manufacturer part number: 82635DSITR50P

    0
    Comment actions Permalink
  • Roman Leuzinger

    Is the interposer 82635DSITR50P the original part from the D405?

    What part is used in the D435?
    According datasheet the interposer of D435 is not straight and is different from the listed part. That one might fit better in our design.

    0
    Comment actions Permalink
  • MartyG

    Are you referring to the interposer in the image below, please?  If so then this flex inteposer is a flexible cable instead of a rigid square circuit board, which is useful for integration into product casings where using a rigid board to connect the D4 and the Depth Module would not be possible due to the internal dimensions of a casing and the other components within it. 

     

    This interposer cable can be ordered from Cocom Consumer Electronics at the contact details provided earlier in this discussion, or you can construct your own using the pin-out and 50-pin connector receptacle details in the data sheet. 

     

     

    In addition, FRAMOS stock pre-made flexible 400 Series interposer cables under the HSF component name in a range of cable sizes referring to their length in mm (HSF50, HSF100, HSF150, HSF200).

    https://www.framos.com/en/product-catalog/3d/3d-accessories 

     

    D435 uses a flexible interposer, as shown in the image below.

     

    0
    Comment actions Permalink
  • Roman Leuzinger

    We have opened a D435 to learn more about the integration and it really helped to see its parts.

    I am already in contact with Cocom for the flex interposer. I will get all the details from there. Either we take one of the of the shelf products or we look for a custom made.

    In the D435 we have found some other parts. Question is if the can buy those as well on the market, or if we have to produce them by ourself. It would be helpfull if we can buy those ase well (as they are injecting molding parts).

    The mask on the D430 module.I guess its function is to reduce reflections between cover glass and metal case of the module.

    Snapper on the D430 interposer. I guess its function is to secure the interposer connector from falling out.

    Are those parts availabe on the market?

    0
    Comment actions Permalink
  • MartyG

    The only parts that are available from retail are the camera Depth Module board, Vision Processor D4 board and interposer connector (flexible cable or rigid board).  Customers who are integrating RealSense will need to provide their own equivalent of the other parts.

     

    If you are planning to use a D430 and have access to a 3D printer or can find a company to print an object for you, the 3D printing blueprint at the link below may be helpful as a sensor mask.  It was designed for use with the D435 camera model (which contains a D430 circuit board) and so the holes should align with the D430 sensors.

    https://www.thingiverse.com/thing:5140445

    0
    Comment actions Permalink
  • Roman Leuzinger

    What kind of adhesive layer is used to stick the lens cover into the housing? Is this IP54?

    Why is the NIR filter in front of the lens cover? Will there be problems if the NIR filter is mounted behind the lens cover?

    Which adhesion layer is used to stick the NIR filter to the lens cover?

    1
    Comment actions Permalink
  • MartyG

    All of that information is related to the camera manufacturing process and so the details will not be available publicly, unfortunately.  All technical information that is publicly shareable is in the data sheet document for the 400 Series cameras and system integrators will create their own solutions for aspects of the assembly that are not covered by the data sheet.

     

    However, the data sheet recommends thermal double-sided adhesive for mounting the depth module and so such adhesive tape would be worth considering for attaching the lens cover to the housing and applying for the edges of the filter outside of the sensor hole.

    0
    Comment actions Permalink
  • Deepak Kumar

    Hi Roman Leuzinger, were you able to gather any information regarding the adhesive layer for mounting of the NIR filter on the cover window. 

    0
    Comment actions Permalink
  • Roman Leuzinger

    Not other than recommended in the datasheet. 
    We have a source but many options to choose from.

    0
    Comment actions Permalink
  • Deepak Kumar

    Thanks Roman Leuzinger for responding. By many options did you mean the adhesive tapes ?

    0
    Comment actions Permalink

Please sign in to leave a comment.