RealSense Support

Intel RealSense D455 object detection within defined window

Comments

5 comments

  • MartyG

    Hi Andrew John Madey  If you do not require identification of specific objects, the most straightforward approach may be a C++, Python or C# language script in the RealSense SDK that applies a post-processing filter called a threshold filter.  This enables you to set a minimum and maximum distance from the camera that Z-depth detail will be rendered at and exclude from the image the depth data that is outside of that defined range.

     

    Examples of creating a bounding box in C++, Python or C# can be found at the link below.

    https://github.com/IntelRealSense/librealsense/issues/5964#issuecomment-594372943

     

    If you would also like to define an XY "region of interest" where depth data outside of that horizontal and vertical area of the image is excluded from the image then this will be more complicated.  It is possible to do so with a bounding box, as described here:

    https://github.com/IntelRealSense/librealsense/issues/2016

     

    If your preference is to use Open3D then a method of cropping an RGBD image is suggested here:

    https://github.com/isl-org/Open3D/issues/2223

    1
    Comment actions Permalink
  • MartyG

    You can also define a threshold filter in the RealSense Viewer tool without requiring any programming.

     

    If you plan to use both RGB and depth and would like to exclude RGB detail by distance as well as depth then you could align depth to color so that the color coordinates are added or removed as the matching depth coordinates are included or excluded from the image.  The rs-align-advanced C++ example program demonstrates this principle.

    https://github.com/IntelRealSense/librealsense/tree/master/examples/align-advanced

    1
    Comment actions Permalink
  • Andrew John Madey

    Hi Marty,

     

    Thanks! I guess the question from there would be, do you know of a way to tabulate the number of such objects observed, automatically?

    I'm trying to figure out if there's a way to automate the counting process so that, per frame, I could figure out how many objects there are, and not have to do it by hand each time (several hundred possible).

     

    Thanks!

    Andrew

    0
    Comment actions Permalink
  • MartyG

    An OpenCV tutorial in the link below for detecting coins on an RGB image and counting them may be adaptable for your application.

    https://medium.com/analytics-vidhya/detecting-and-counting-objects-with-opencv-b0f59bc1e111

    0
    Comment actions Permalink
  • Andrew John Madey

    Thanks!

    0
    Comment actions Permalink

Please sign in to leave a comment.