View my account

New Error with New 435 Delivery: Auto Gain Limit

Comments

12 comments

  • Steve Steve

    I pulled the 05.13.00.50 version from here:
    https://www.intelrealsense.com/developers/

    0
    Comment actions Permalink
  • MartyG

    Hi Steve Steve The Auto Gain Limit limits the maximal digital gain value used in Auto-Exposure.  Its value can be set from 16 to 248.  Default is 0 which means full gain.  If the requested gain limit is less than 16, it will be set to 16.  If the requested gain limit is greater than 248, it will be set to 248.

     

    The error message suggests that the camera was not ready to be queried regarding the Auto Gain Limit at the moment that the setting was requested by the RealSense Viewer tool.

     

    Firmware 5.14.0.0 is available for download from the RealSense firmware releases page.  It is recommended for use with the recently released RealSense SDK version 2.53.1

    https://dev.intelrealsense.com/docs/firmware-releases#d400-series-firmware-downloads

     

    Firmware version 5.13.0.50 is recommended for use with SDK version 2.50.0 and 2.51.1

     

    The Spec Update firmware release notes document contained in the zipped firmware folder does not list any changes in the Summary Table of Changes for the 5.14.0.0 firmware.

     

    RealSense firmware drivers are extensively tested before release.  If firmware stability remains a concern for customers though because it will be used in a critical application or commercial product then there are a couple of options that can be considered.

     

     

    1.  Use a Recommended production camera firmware version.  The most recent firmware classified as Production (proven stability for commercial / critical applications) at the time of writing this is 5.13.0.50

    https://dev.intelrealsense.com/docs/recommended-production-camera-configurations

     

    2. Alternatively, apply a rule of 'one version back' by using a RealSense SDK and firmware combination that is one version older than the latest versions.  This will allow time to see whether any issues emerge in a newly released firmware before later adopting it.

    0
    Comment actions Permalink
  • Steve Steve

    Thanks MartyG
    Following up, two questions

    FIRST:
    Is it standard procedure to ship new cameras with non-production versions of firmware?--should we expect that in the future?
    I didn't receive the package, was there something there to indicate the change in the current delivery? --something that might have been missed or ignored by our assembly team?

    SECOND:
    You said: 

    "The error message suggests that the camera was not ready to be queried regarding the Auto Gain Limit at the moment that the setting was requested by the RealSense Viewer tool."

     

    • Since the error does NOT occur with 5.13.00.50, is this query new.
      (All of the new cameras received are failing)

    • Assuming the query exists in the previous production version 5.13.00.50..
      Then, is the response timer expiring too fast for current production 435s (As these are new)?
      Or, is the hardware different?


    (Something changed--but I don't see it in the 5.14 release documentation.  So, Heads-Up I guess?)

    0
    Comment actions Permalink
  • MartyG

    Auto Gain Limit was introduced in February 2021 in SDK version 2.42.0.

     

    Firmware 5.14.0.0 was only released at the start of December 2022, within the past 2 weeks at the time of writing this.  Typically, new units of existing camera models do not have the latest firmware.  Is it possible that your assembly team may have manually updated all the cameras to firmware 5.14.0.0 in the RealSense Viewer after having received the batch?

     

    I would recommend updating one of the cameras to 5.14.0.0 using the firmware file downloaded from the firmware archive page and see whether the error re-occurs with that particular camera.  Also please bear in mind that this firmware is intended for use with SDK 2.53.1

     

    0
    Comment actions Permalink
  • Steve Steve

    Great...if it's unusual to ship a non-production Firmware version, I'll sleep better at night !  :)

    Not a chance our assembly team updated to 5.14 themselves.
    They only know how to update in the RealSense software--and it's still set to 5.13.00.50
    (and as I pointed out...5.13.00.50 is what is available from the main developer page, rendering the other somewhat obscure)

     

    I can try updating one of my cameras to 5.14 and let you know what happens.

     

     

     

     

     

    0
    Comment actions Permalink
  • MartyG

    Thanks very much.  I recommend obtaining firmware bin files directly from the firmware releases page in future.

    https://dev.intelrealsense.com/docs/firmware-releases

    0
    Comment actions Permalink
  • Steve Steve

    I updated to 5.14 from the suggested directory.
    Upon restarting RealSense software (v: 2.49.0.3474)...I immediately get the Auto Gain Limit Error
    (Restored defaults > no improvement)


    I updated back down to 5.13.00.50, and the error stops.


    0
    Comment actions Permalink
  • MartyG

    Firmware 5.14.0.0 is intended for use with RealSense SDK version 2.53.1.  If your project is unable to upgrade its SDK version from 2.49.0.3474 then I recommend continuing with 5.13.00.50.  As the firmware documentation lists no feature / bugfix changes for 5.14.0.0, using 5.13.00.50 is unlikely to disadvantage you.

    0
    Comment actions Permalink
  • Steve Steve

    I agree...and my original concerns don't seem to be an issue.

    At this point, I only mention as this error occurs in the RealSense Software (outside of our project)

    I've updated our team...
    We can close this out.
    I really do appreciate your help!!

    0
    Comment actions Permalink
  • MartyG

    You are very welcome.  Thanks very much for the update! 

    0
    Comment actions Permalink
  • Ojeda

    The same happened with the 405 camera.

    So far the error disappears with the installation of https://github.com/IntelRealSense/librealsense/releases/tag/v2.53.1

    0
    Comment actions Permalink
  • MartyG

    Thanks very much Ojeda for your report.  Firmware version 5.14.0.0 is the recommended firmware for use with SDK version 2.53.1.

    0
    Comment actions Permalink

Please sign in to leave a comment.