RealSense Support

Changing Fov by cropping images on D405 depth camera

Comments

3 comments

  • MartyG

    Hi Luke Bowersox  The data sheet does not list the 848x100 and 300 FPS mode.  It is designed for use only with models equipped with a fast global type shutter on the depth sensor such as D435 / D435i / D435f and D455.  The D405 does though also have a global shutter on its depth sensor.

     

     

    I confirm that the D405 does not list 848x100 / 300 FPS as a supported depth resolution in the RealSense Viewer.  It is listed in the Viewer as selectable for D435 / D435i / D435f and D455.  

     

     

    Instead of looking up configurations in the data sheet, entering a particular resolution and FPS combination into the Viewer's options side-panel is a quick and easy way to find out whether that configuration is supported on the specific camera model that you are using.  If a combination is unsupported then the settings will automatically change to a different suggested configuration, whilst if it is supported then the resolution and FPS settings will not change,

     

    It is not possible to define a custom field of view size to replicate the 848x100 "center strip" letterbox view but as you suggest, a depth image can be cropped in the X and Y axes.  This can be done by defining a bounding box that excludes from the depth image all data outside of the box.  This can be a complicated procedure though, as described at the link below.

    https://github.com/IntelRealSense/librealsense/issues/2016#issuecomment-403804157

    0
    Comment actions Permalink
  • Luke Bowersox

    Marty!

    Thanks so much for this tip. It saved me a ton of legwork on my part.  Good to know the difference between the global and rolling shutter camera capabilities.

    Best,

    Luke

    0
    Comment actions Permalink
  • MartyG

    You are very welcome, Luke  :)

    0
    Comment actions Permalink

Please sign in to leave a comment.