D455 No Buffer Space Available
Hello Dear Community,
Recenlty I bought 8 pcs D455, 7 of them is working well but one of them not recognize neither windows 10 nor ubuntu 18.04.
I think It's firmware issue.
After that problem, what I try:
- Change USB ports from 3.0 to 2.0
On Windows: USB-3.0 = Unkown Device
USB-2.0 = (!)Intel(R) RealSense(TM) Depth Camera 4n0 Depth
Device Manager: Device not started Code:10 (
Device USB\VID_8086&PID_0AD6&MI_00\9&13f6c9c4&0&0000 was configured.
Driver Name: winusb.inf
Class Guid: {88bae032-5a81-49f0-bc3d-a4ff138216d6}
Driver Date: 06/21/2006
Driver Version: 10.0.19041.1
Driver Provider: Microsoft
Driver Section: WINUSB.NT
Driver Rank: 0xFF2000
Matching Device Id: USB\MS_COMP_WINUSB
Outranked Drivers: usbvideo.inf:USB\Class_0e:00FF2003
Device Updated: false
Parent Device: USB\VID_8086&PID_0AD6\8&2efe0359&0&1
)
Which realsense-viewer give me Please Connect Intel Realsense Camera!
On Ubuntu 18.04:
lsusb shows: Bus 004 Device 002: ID 8086:0af5 Intel Corp.
realsense-viewer: 04/11 21:11:36,379 WARNING [140125751576448] (enumerator-libusb.cpp:45) failed to read USB config descriptor: error = -1
rs-fw-update:
Nothing to do, run again with -h for help
04/11 21:12:46,344 WARNING [139762838251200] (enumerator-libusb.cpp:45) failed to read USB config descriptor: error = -1
There are no connected devices
04/11 21:12:46,345 WARNING [139762838251200] (enumerator-libusb.cpp:45) failed to read USB config descriptor: error = -1
How can I work with that Camera?
Thanks for reading that topics.
Best Regards
Please sign in to leave a comment.
Comments
1 comment