RealSense Support

Comments

25 comments

  • Yu-Chern Peh

    Hi E5119121b0,
     
    Yes, it is available in the link previously but now it has been removed. However, source code is still available which allows you to build. 
     
    You can refer to the tutorial below:
    https://github.com/IntelRealSense/RealSenseID/tree/master/tools
     
     
    Regards,
    Yu Chern

    0
    Comment actions Permalink
  • E5119121b0

    Thanks for your cooperation. Mr.(or Ms.) Yu-Chern Peh.
    However, when I tried to build at the command prompt on the introduced site, I did not know the directory name after "cmake .." in "Default build".
    Could you please let me know if you know?

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi E5119121b0,

     

    It depends on where you download or clone the repository.

    For example, I clone the RealSenseID repository in Desktop directory. I need to navigate to the cloned folder located in Desktop directory (cd Desktop\
    RealSenseID) in the command prompt first (same meaning as Step 2:In cloned folder, open command line).

    Next, I create a folder named as "build", which now the "build" folder is located in Desktop\RealSenseID\build directory.

    Then, you can proceed to the remaining build steps. 

     

    Regards,

    Yu Chern

    0
    Comment actions Permalink
  • E5119121b0

    Thank you.
    However, when I try to start ”rsid-viewer.exe", the app does not open for some reason (it quits instantly after starting).
    Do you know why?

    0
    Comment actions Permalink
  • E5119121b0

    I'm sorry. I will add it.

    When I entered rsid-cli.exe <port> with reference to the "RealSenseID command line tool" item on the example site, It says "cannot run on your PC".

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi E5119121b0,

    Please make sure you are assigning to the right port.

    Run Windows "Device Manager" and check in which COM port the device was recognized (It should appear under Ports (COM & LPT) (For example: COM3)

    Which OS you are using and your PC spec?

     

     

    Regards,

    Yu Chern

    0
    Comment actions Permalink
  • E5119121b0

    It is as follows
    edition: Windows 10 home
    version: 21H2
    OS build: 19044.2130

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi E5119121b0,

    I suspect the issue might due to incompatible of the firmware version. 

    I am expecting you downloaded the latest RealSense ID SDK version (0.25.0).
    Please try to upgrade the firmware version(F450_4.3.0.8200_SKU1_SIGNED.bin) using rsid-fw-update.exe (located in RealSenseID\build\bin\Debug).

    Command in command prompt:

    rsid-fw-update.exe --file <path>/F450_4.3.0.8200_SKU1_SIGNED.bin --port <COM#>


    You might need to force upgrade the firmware version to 3.1 ( F450_3.1.0.29_SKU1_SIGNED.bin ), if you received the following errors,

    Firmware cannot be updated directly to the chosen version.
    Flash firmware version 3.1.#.# first.

    Command in command prompt:

    rsid-fw-update.exe --file <path>/F450_3.1.0.29_SKU1_SIGNED.bin --port <COM#> --force-version

    rsid-fw-update.exe --file <path>/F450_4.3.0.8200_SKU1_SIGNED.bin --port <COM#>

     

    Regards,

    Yu Chern

    0
    Comment actions Permalink
  • E5119121b0

    I'm sorry.

    Returned that the syntax of the command was incorrect

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi E5119121b0,

    You have to edit the command based on the downloaded bin file directory and the according port.

    For example, 

    rsid-fw-update.exe --file Downloads\F450_4.3.0.8200_SKU1_SIGNED.bin --port COM3

     

     

    Regards,

    Yu Chern

    0
    Comment actions Permalink
  • E5119121b0

    Thank you.

    But, It returned "Invalid firmware file!"

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi E5119121b0,

    Have you download the firmware file (.bin file)? I have hyperlinked the firmware file to its download page. 

    F450_4.3.0.8200_SKU1_SIGNED.bin

    If you already downloaded the firmware file, please ensure you are assigning to the right port.

     

     

    Regards,

    Yu Chern

    0
    Comment actions Permalink
  • E5119121b0

    I'm sorry.

    "[2022-10-28 15:54:19.456] [debug] [WindowsSerial] Opening serial port COM4
    [2022-10-28 15:54:19.738] [debug] [WindowsSerial] Closing serial port
    Invalid firmware file!” was returned.

     I completed and confirmed Port and file download.

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi E5119121b0,

     

    Thanks for confirming. I am sorry that I only available to test the installation of the latest RealSense ID SDK version (0.25.0) on my side next week. 

    In a meanwhile, you can try with RealSenseID SDK version v0.23.0 if you are willing to do so.

    Download RealSenseID SDK version v0.23.0 (https://github.com/IntelRealSense/RealSenseID/tree/v0.23.0) or clone the repository: git clone -b v0.23.0 https://github.com/IntelRealSense/RealSenseID.git

     

     

    Regards,

    Yu Chern

    0
    Comment actions Permalink
  • E5119121b0

    I will try.

    Thank you very much.

    0
    Comment actions Permalink
  • E5119121b0

    excuse me.

    I tried several times after that.
    But, Failed.
    "[2022-11-04 01:35:29.619] [debug] [WindowsSerial] Opening serial port COM4
    [2022-11-04 01:35:29.626] [error] [DeviceControllerImpl] Failed to open serial port. GetLastError: 2” was returned.
    Do you know why?

    0
    Comment actions Permalink
  • E5119121b0

    I'm sorry. Append.
    After that I tried.
    It looks like the update was successful. (After entering ``rsid-fw-update.exe --file <path>/F450_3.1.0.29_SKU1_SIGNED.bin --port <COM#> --force-version'', ``Firmware update finished successfully'' was returned.)
    But, it still won't start.

     

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi E5119121b0,

     

    Next update the firmware to the latest, F450_4.3.0.8200_SKU1_SIGNED.bin.

    rsid-fw-update.exe --file <path>/F450_4.3.0.8200_SKU1_SIGNED.bin --port <COM#> --force-version

     

    I have validated the installation of the latest RealSense ID SDK version (0.25.0). The rsid-viewer is running well on my side. 

     

     

    Regards,

    Yu Chern

    0
    Comment actions Permalink
  • E5119121b0

    I'm sorry.

    After that I tried this.
    But, it still won't start.

     

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi E5119121b0,

     

    I'm sorry, I didn't catch that. Could you provide any screenshot or error message?

     

     

    Regards,

    Yu Chern

    0
    Comment actions Permalink
  • E5119121b0

    I'm sorry. The explanation was insufficient.

    "rsid-fw-update.exe --file <path>/F450_4.3.0.8200_SKU1_SIGNED.bin --port COM4 --force-version" "Firmware update finished successfully" was returned. It looks like the update was successful. However, even after that the Viewer did not start.

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi E5119121b0,

     

    Do you mean the ”rsid-viewer.exe" still quits instantly after starting or no response after opening?

    Please try opening rsid-viewer.exe with command prompt or run rsid-viewer.exe as administrator (right-click).

    Besides, please also try running rsid-cli.exe.

     

     

    Regards,

    Yu Chern

    0
    Comment actions Permalink
  • E5119121b0

    It will appear momentarily on the taskbar but will close immediately.
    I tried the above method but it didn't work.

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi E5119121b0,

     

    Please try troubleshooting the issue by referring to the following YouTube videos:

    HOW TO FIX EXE FILES NOT OPENING, SETUP.EXE CRASHING

    How to Fix EXE File is Not Opening Windows 10: EXE File Opener

     

     

    Regards,

    Yu Chern

    0
    Comment actions Permalink
  • E5119121b0

    I will try.

    Thank you very much.

     

    0
    Comment actions Permalink

Please sign in to leave a comment.