RealSense Support

3D Field Reconstruction

Comments

3 comments

  • MartyG

    Hi Yuval Arnon  If you are able to compile computer code then the RealSense SDK's rs-kinfu C++ open-source example program may be helpful.  It enables a single camera to be moved around a scene, progressively building up a point cloud scan with frame fusion.  Once you are satisfied with the level of detail on the scan then you can export the pointcloud to a .ply format pointcloud data file.

    https://github.com/IntelRealSense/librealsense/tree/master/wrappers/opencv/kinfu

     

    If you do not wish to reconstruct the data in real-time but instead scan and then do work on the saved data later then the RealSense SDK's free and open-source RealSense Viewer tool provides the ability to record a continuous stream as a bag file (which is like a video recording of camera data) or as single-frame ply pointcloud file.  Multiple ply files exported from the Viewer could be 'stitched' together into a single large pointcloud that incorporates all of the recorded viewpoints.

     

    The RealSense SDK can treat a bag file as though it is a live camera, making it easy to do work with the data using existing publicly available scripts.

     

    Using the RealSense Viewer tool has the advantage that it is available in pre-built executable form and so programming knowledge is not required in order to use it.  The Viewer can also load in bag files recorded with it and perform further work on the data in real-time via an easy to use graphical interface, such as applying post-processing filters.

    0
    Comment actions Permalink
  • MartyG

    Multiple .ply pointcloud files exported from the Viewer could be stitched together using a free open-source tool called CloudCompare (available on Linux via a Snap package if you do not have access to Windows).

     

    https://cloudcompare.org/forum/viewtopic.php?t=2543

    https://www.danielgm.net/cc/

    http://www.cloudcompare.org/doc/wiki/index.php?title=Merge

    Linux snap package
    https://snapcraft.io/cloudcompare

    0
    Comment actions Permalink
  • Yuval Arnon

    Hi MartyX Grover Thank you for the comment and details, I will give it a try. 

    0
    Comment actions Permalink

Please sign in to leave a comment.