[Question] product recognition failure occurs after a certain period of time( D405)
Hi.
we use D405 devices for Windows10 or Linux with USB3.0 interface.
when i used this device with USB 3.0 interface, device recognition failure occurs after a certain period of time.
but USB2.0 interface works well.
Environment]
1. Intel RealSense D405
2. OS : Windowns 10 or Ubuntu
3. Test App: Intel RealSense Viwer.
4. Symptom: device recognition failure after a certain period of time.(few days)
If you have any information about this symptom. please let me know.
Best regards
Powell Chang
-
Hi Powellchang RealSense 400 Series cameras have been tested by Intel for long-,running and can operate for an indefinite period of time so long as their operating temperatures remain within the recommended maximum range. If the camera has been active for 3 days before a problem manifests then it is likely that it is occurring due to a cause other than the camera hardware. This could include a glitch on the USB port or cable, the computer hardware or the computer's operating system.
As you report that the camera works well on USB 2 but has the detection-loss issue on USB 3, that would seem to indicate that it is an issue related to the USB system rather than camera temperature, operating system or a computer hardware issue other than USB.
If it occurs on different PCs (Windows and Ubuntu) then that reduces the likelihood of it being a problem with the USB ports or the USB controllers.
A factor common to all of the computers would be the camera's USB cable. Are you using the official 1 meter cable supplied with the camera or a longer cable of your own choice, please? Also, is the camera's casing hot to the touch when the detection issue occurs, as a hot casing could also indicate a USB cable problem.
-
HI MartyG
we are using the official 1-meter cable supplied with the RealSense.
I will change Computer and test again,
if the same issue happens, I will update you.
Best regards
Powell Chang
-
Thanks very much, Powellchang
Please sign in to leave a comment.
Comments
3 comments