949001994
- Total activity 19
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Comments
Recent activity by 949001994-
Thank you so much, that's what I mean (so I can exclude d435f and buy d405)! In addition, can t265 obtain an image without spots such as d405 in this case?
-
This comparison shows the effect! But I mean I hope that when I turn on the emitter enabled option on the d435i placed above, does the image presented by the d405/d435f binocular have this spot, as...
-
Thank you very much, and I don't have to exclude infrared frequencies from being visible to the camera,I just want to buy a binocular image without spots.Maybe D435f be better because it has the sa...
-
Hello, sorry to disturb you again. I want to confirm with you again whether the d435f/d405 can be installed in the above way, whether the binocular camera cannot receive the speckle emitted by d435...
-
Thank you so much for your serious answer! be deeply grateful!
-
Thank you very much for your reply! My question is that when two d435i are placed as shown in the above picture, the lower d435i has turned off the emitter enabled option, and the upper one has tur...