Henry
- Total activity 11
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 4
Posts
Recent activity by Henry-
D401 module questions
I have used the D405 camera and have some questions on switching to the D401. 1) If I buy the D401 camera module and the D4 vision board for the D401, is the calibration data stored on the D4 visio...
-
D435 vs D405 IR lens comparison
I'm trying to understand performance of the images produced by the D405/D401 vs the D435. The raw D405 IR image seems much sharper than the D435 which I can say is blurry. Is this due to it bein...
-
D405 Focus and Depth of Field vs D430?
What are the lengths that the D405 RGB camera can resolve clearly vs the D430? I have a D430 and lengths of around 120mm it appears pretty blurry in the RGB but still usable though not ideal. Eg ...
-
Confusion about Camera Extrinsics and how to use
I want to utilize the Color camera and make some coordinate transforms using AprilTags for depth to compare against the Intel camera distance measurements. 1) I grab an color and a depth image. I ...