Michael Harder
- Total activity 10
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 1
- Subscriptions 4
Activity overview
Latest activity by Michael Harder-
Michael Harder created a post,
How to access the translation parameter of T265 via python and openCV
Hello, we need to access the position vector of the T265 camera in openCV: We already have pyrealsense2 installed. How can we access this "Translation" parameter in openCV and python? Thank you v...
-
Michael Harder created a post,
How to analyze IR (850nm) wavelength with the Intel RealSense D435 and IR-pass filter
In our actual project we have multiple IR lights and Intel D435 cameras. We need to capture the IR video stream with the RealSense cameras. Our Region of Interest has a size of about 100 x 100 mm a...
-
Michael Harder created a post,
Zooming with the IR Imagers of the RealSense D435
We have multiple Intel RealSense D435 cameras. For a project we are streaming the video of one of the two IR imagers. We have to use the imagers, because we also need to analyze the IR part. Does t...
-
Michael Harder commented,
Hello MartyG, thank you very much for this detailed answer. I really appreciate it. I will check this guide out and also bought an linear polarization filter. Just to be sure, there is no official ...
-
Michael Harder created a post,
IR light with Intel RealSense Depth Camera D435
Hello, we have two D435 cameras an we really like them. We want to use them for a vision project, in which infrared light is used. We want to use IR lights and capture the IR wavelength. So we are ...