Juntea Kim
- Total activity 8
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Activity overview
Latest activity by Juntea Kim-
Juntea Kim commented,
Thank you for the guidance. Following your instructions, I checked the metadata overlay in RealSense Viewer while the camera was operating in Mode 0. The Hardware FPS value was checked at three dif...
-
Juntea Kim commented,
Thank you for the suggestions. I tested finer external-trigger frequency adjustment in Mode 2 using the official RealSense Viewer. Test configuration:- D455 firmware: 5.17.3.10- RealSense Viewer / ...
-
Juntea Kim commented,
Thank you. I completed the requested Mode 0 comparison in the official RealSense Viewer and also performed an additional Mode 2 test with Global Time disabled. Every recorded depth frame was analyz...
-
Juntea Kim commented,
Thank you. I have now repeated the test using the official RealSense Viewer and analyzed every recorded depth frame offline. This test reproduced the depth gaps in the Viewer itself, so I need to c...
-
Juntea Kim commented,
Thank you for the clarification. The D455 is using the official 1-meter USB cable supplied with the camera, not a third-party cable. For the Viewer test described above, it was connected directly t...
-
Juntea Kim commented,
Thank you for the detailed response. I repeated the test after power-cycling the system because the previous run was interrupted by a loss of power. The sync cable is approximately 20 cm long (abou...
-
Juntea Kim created a post,
[D455] Depth stream stalls for up to 2.4 seconds in Inter Cam Sync Mode 2 at 1280x720@15
Hello RealSense Support, I am experiencing repeated long stalls in the depth stream of a RealSense D455 while using Inter Cam Sync Mode 2 (Slave). Mode 2 is being used according to the documented...