JIshnu S
- Total activity 6
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Activity overview
Latest activity by JIshnu S-
JIshnu S commented,
MartyX Grover , we tried -DBUILD_WITH_CUDA=ON but dont we any difference in gpu usage
-
JIshnu S created a post,
High Latency in RealSense ROS1 Node with D435 on Jetson Xavier NX at 15 FPS
We are testing Intel RealSense D435 depth streaming on a Jetson Xavier NX using the ROS1 dcam node and are observing unexpectedly high end-to-end latency, even though the camera is only running a...
-
JIshnu S commented,
Heyy MartyX Grover , I have set a very low exposure for color sensor , ie 10 micro seconds . Isnt 12 cm (60 ms in time) of misalignment too high when exposure is a very low value like this? Rolling...
-
JIshnu S created a post,
Misalignment in depth and color image with D435
We are using D435 camera to capture an object moving at 2 meter/sec . Here the color and corresponding depth image has a misalignment of around 12 cm . Is this expected with this camera model ? Is ...