Wildanazman072
- Total activity 12
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Activity overview
Latest activity by Wildanazman072-
Wildanazman072 commented,
Yes, I already checked every time I use the camera. I only run one application at a time. I will try to use it on raspberry pi 4 later on. does it use the same setting as Linux?
-
Wildanazman072 commented,
Here's my firmware version.
-
Wildanazman072 commented,
tried the method. but still no output from camera.
-
Wildanazman072 commented,
I tried another cable, the output is the same. nothing showed. I believe the cable is not the problem.
-
Wildanazman072 commented,
Could the problem probably related to type c wire I'm using? because I'm using my phone's type c since I did not get any wire when I bought the camera online. However, the camera's working fine in ...
-
Wildanazman072 commented,
Yes, I'm using windows. Only have a change camera button and it only changes between the depth camera and RGB camera. But both do not output anything.
-
Wildanazman072 commented,
Yes, I already try the camera in RGB mode, the result is the same for both RGB and depth.
-
Wildanazman072 commented,
The device is available but as you can see there is no output from the camera. Same goes when I used google meet.
-
Wildanazman072 created a post,
Intel Realsense d435
Hi, can I use my intel realsense as a webcam. For example, I want to use the intel realsense d435 for my face recognition project (python) which previously use a logitech webcam. Can I use intel re...
-
Wildanazman072 created a post,
Intel Realsense d435 face recogntion
Hi and a very good day, Are there any samples on face recognition using openVINO toolkit for Intel Realsense d435? For now, I only found face detection for the intel realsense but not face recognit...