Wildanazman072

  • Total activity 12
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 2

Activity overview

Latest activity by Wildanazman072
  • Wildanazman072 commented,

    Yes, I already checked every time I use the camera. I only run one application at a time. I will try to use it on raspberry pi 4 later on. does it use the same setting as Linux?

  • Wildanazman072 commented,

    Here's my firmware version.

  • Wildanazman072 commented,

    tried the method. but still no output from camera.

  • Wildanazman072 commented,

    I tried another cable, the output is the same. nothing showed. I believe the cable is not the problem.

  • Wildanazman072 commented,

    Could the problem probably related to type c wire I'm using? because I'm using my phone's type c since I did not get any wire when I bought the camera online. However, the camera's working fine in ...

  • Wildanazman072 commented,

    Yes, I'm using windows. Only have a change camera button and it only changes between the depth camera and RGB camera. But both do not output anything.

  • Wildanazman072 commented,

    Yes, I already try the camera in RGB mode, the result is the same for both RGB and depth.

  • Wildanazman072 commented,

    The device is available but as you can see there is no output from the camera. Same goes when I used google meet.

  • Wildanazman072 created a post,

    Intel Realsense d435

    Hi, can I use my intel realsense as a webcam. For example, I want to use the intel realsense d435 for my face recognition project (python) which previously use a logitech webcam. Can I use intel re...

  • Wildanazman072 created a post,

    Intel Realsense d435 face recogntion

    Hi and a very good day, Are there any samples on face recognition using openVINO toolkit for Intel Realsense d435? For now, I only found face detection for the intel realsense but not face recognit...