Rachel Cheng
- Total activity 4
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Posts
Recent activity by Rachel Cheng-
more noise at 1 m distance than 0.5 m
Hi, I was wondering why the L515 shows more noise when scanning an object at 1meter distance than at 0.5 m. There was no sunlight in the room, the same presets were used (Short range and no ambient...
-
can't scan concave surface
Hello, I've been trying to scan the concave surface of a styrofoam sphere. When I export the scan as a ply file and examine the point cloud, it doesn't look like a sphere. What is the reason why th...