cam test

  • Total activity 8
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by cam test
  • cam test commented,

    MartyX Grover Ok, will try out on GitHub. As regards the sensor/ISP capabilities, is there a reg that can put the ISP in a test-pattern mode? This would be a helpful capability for debugging.

  • cam test commented,

    In this case, it seems that something would be missing or different in the configuration made by using the commands exposed in the mipi-camera-driver repo and the WRs done by using the librealsense...

  • cam test commented,

    MartyX Grover Yes, I'm using a v4l2 streaming app (qv4l2). In case of the streaming app, I compared the ones when using the USB-based paths and its drivers, and they contained the same video qualit...

  • cam test commented,

    Hi MartyX Grover,   Ok, the resulted frame from the RealSense D457 is like this one (using the YUYV format in the V4l2-related streaming app - 1280x720@30fps, being the same in case of using other ...

  • cam test commented,

    MartyX Grover Yes, but in case of the final format that is resulted after the ISP-based conversion, is this one a YUV422 one [UYVY8_1x16 - Packed YUV 4:2:2, 8 bits per component and 2 bytes/pixel -...

  • cam test commented,

    MartyX Grover Yes, I'm using the deserializer from the example design that is hosted on GitHub. The previously mentioned error was because of the wrong usage when doing a manual setup of the device...

  • cam test created a post,

    D457 module reg-related issues (GMSL)

    Hi, I'm using the D457 module along with the GMSL-based setup. All the communication-related things between the serializer/deserializer devices are running successfully, but the modules' registers...