Jsadural
- Total activity 9
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Comments
Recent activity by Jsadural-
Hello Dan, I did notice that the RGB acted as the master and IR as a slave as I varied the frame rates. I did see some option to turn IR as the master but that did not do what I was hoping, to dec...
-
Hello Dan, Thank you for that information, it was exactly what I was looking for. I took your suggestion and ran at 90fps with a shutter setting of 9900 and was able to detect my pulse very dependa...
-
Hello Dan Nie, Thank you for your response but for my scenario, I do not have the luxury of knowing when the pulse is going to happen. Imagine someone shooting a laser at a wall, it's all luck of ...
-
The laser is at 780nm wavelength and pulse duration of 6ms. A long duration 780nm wavelength pulse at 40ms duration is detected visually and algorithmically no problem whether directed at the came...
-
So my scenario of detecting a flashing LED is really just an analogy for measuring a short pule duration IR laser being shot at a wall that the camera is pointed at. I am shooting a laser that has...
-
You are correct, it is an IR led light flashing in the room and is completely independent from the camera. From what I understand, HDR is the combination of short and long exposure images. I don'...
-
Thank you for your post but it does not directly address the issue I am experiencing. I am trying to detect the flickering IR led with the "IR camera only." I am unable to set the exposure to exa...