Waddelat

  • Total activity 2
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Posts

Recent activity by Waddelat Recent activity Votes
  • D455 accuracy and frame rate

    Hi Can i used the D455 to capture objects at 300 fps as in D435?. Also, I read that D455 has higher accuracy compared to D435? So if the camera is 1m from the object, what is the expected accuracy ...