Waddelat
- Total activity 2
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Activity overview
Latest activity by Waddelat-
Waddelat created a post,
D455 accuracy and frame rate
Hi Can i used the D455 to capture objects at 300 fps as in D435?. Also, I read that D455 has higher accuracy compared to D435? So if the camera is 1m from the object, what is the expected accuracy ...