Marty Grover

  • Total activity 20
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 9

Comments

Recent activity by Marty Grover Recent activity Votes
  • NaN is 'Not a Number', an erroneous value.  But as your RGB stream is working, unless you are performing an application where extrinsic values are important such as aligning depth and RGB images to...

  • Sometimes installations of the SDK on Jetson can work without applying the L4T patch script.  Are you able to achieve a working SDK installation if you skip the patch script installation step, plea...

  • I'm pleased to hear that you received a shipping notification.   Instructions on order tracking are included in an email that will be sent to you when your order ships.  You can check the status of...

  • You are very welcome.  Please let me know if you need additional information and I will be happy to help if it is possible to offer advice outside of an NDA.

  • It sounds as though detection of the RGB sensor by the firmware driver during connection of the camera is erratic.  When a hardware reset is performed, the camera automatically disconnects and then...

  • Yes, the downgrade lock is permanent and only replacing the camera or changing the D4 V3 board of your existing camera can restore the allowed downgrade count back to 20. As mentioned in your earli...

  • I located a reference which has an example of a diagram of the depth FOV triangle whose origin is the left-side IR sensor. https://github.com/realsenseai/librealsense/issues/2355#issuecomment-41871...

  • Hi Laurin Steiner  I would recommend not attempting to calculate your own FOV diagram or considering the invalid depth band due to the complexities involved.  It is much easier to work out the dept...

  • You are very welcome!   The angle of the projection does not matter so long as a visible pattern is being cast onto the surface.    It has to be a visible projection, like the one from the USB proj...

  • The MIPI platform driver works without modification on Jetson AGX Xavier and Orin.  There is not information available though about how it performs on other Jetson models or steps require (if any) ...