Iolcoz
- Total activity 10
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Activity overview
Latest activity by Iolcoz-
Iolcoz created a post,
Given Intel D435 when set_region_of_interest then sometimes error occurred
Environment: Intel D435 camera, pyrealsense library Operation condition: we are continuously getting frames from the camera by calling to the method wait_for_frames in an execution thread. In anoth...
-
Iolcoz commented,
Thank you. Yes, I was already aware of depth to color alignment importance and it is something that I was already applying in all I have reported. On the other hand, yes, the troublesome surface ...
-
Iolcoz commented,
The problem is that in the context of the application where I am applying this, I cannot ensure or demand a specific location for the two objects because is something that I might not control. What...
-
Iolcoz commented,
In the normal axis, object A is about 50 cm to the camera and object B is about 53 cm to the camera. In the vertical axis, object A is about 3 cm above object B. The ceiling spotlight is behind t...
-
Iolcoz commented,
Yes, I already had the IR Emitter enabled. Sorry for not adding this information in the issue description.
-
Iolcoz commented,
It is an artificial light in the ceiling that illuminates more the surface of object A than the surface of object B. Some areas of the image illuminated by the spotlight seem to be quite saturated,...
-
Iolcoz commented,
Thank you for your fast answer. Yes, I have auto-exposure enabled, both for rgb and depth channels.
-
Iolcoz created a post,
Depth values affected by spotlight
Camera: Intel D435 Firmware: 5-12-7-100 Situation: Given two objects A and B, where object A is a couple of centimeters closer to the camera than object B. Under normal light conditions, the depth ...