Liuruifangshiwo
- Total activity 6
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 1
- Subscriptions 1
Comments
Recent activity by Liuruifangshiwo-
I installed the sdk2.0, and got the sr300 works by installing driver in windows device manager. But the dcm is still not installable.
-
Camera is recgnized now by flashing firmware on intel PC. But DCM still cannot be installed on the Ryzen PC. It might be the problem of the firmware updater.
-
The camera is now recognized as a winUSB device :"USB\VID_8086&PID_0AA5&REV_3150&MI_04"